How to recover the factory state of STM32L051C8T6
Now, I am developing low power LoRa node using STM32L051C8T6.
We can upload the script on the new chip of STM32L051C8T6, and get low current consumption of less than 10 microAmp.
However, for the used chip of STM32L051C8T6, we can upload the same script, and
running well, but the current consumption is about 4 mA, much higher than the new chip.
the used chip of STM32L051C8T6 mean that the chip is in the same batch production, but we have been used for many time uploading the script during development.
I have been full erase the chip, but no result.
Is there any means to recover the factory state of STM32L051C8 so we can consider it as a new chip ?