Skip to main content
OPush
Associate
Nov 7, 2019 9:15 AM UTC
Question

How to implement MLPF-WB55-01E3 with STM32WB55?

Hi,

  1. Should I use 100pF capasitor in series after MLPF-WB55-01E3 for the DC blocking?
  2. Is there full schematic and reference design for STM32WB55 with MLPF-WB55-01E3?

Br, Oleg

This topic has been closed for replies.

2 replies

Remi QUINTIN
ST Technical Moderator
Nov 7, 2019 2:42 PM UTC

The 100pf is only required when your design is planned to support both an SMA connector and an antenna.

If the board only supports an SMA connector, there is no need any additional component.

If the board only supports an antenna, then you need a matching network in between the IPD and the antenna.

Remi QUINTIN
ST Technical Moderator
Nov 7, 2019 2:46 PM UTC

Find below the link of the gerber file for the reference boards with the IPD:

https://www.st.com/en/microcontrollers-microprocessors/stm32-wireless-mcus.html#resource

You can also have a look  at the application note AN5165 ‘Getting_started_HW_RF_development’ for the STM32WBxx board design guidelines

and the datasheet of the IPD MLPF-WB55-01E3 to follow for a correct implementation of the IPD.