Skip to main content
nick.T
Visitor II
Aug 6, 2019 8:14 AM UTC
Question

How to get SWO working on STM32WB55

SWO seems to put the first few bytes into the TPIU fifo, and then the fifo goes to not ready and stays there.

I have the following init code for GPIOB-P3,

/* USER CODE BEGIN 2 */
/* configure Port B3 as SWO, this doesn't seem to get done by cube MX ? */
void SWO_GPIO_Init(void)
{
 GPIO_TypeDef *GPIOx = GPIOB;
 GPIO_InitTypeDef SWO_Init = {0};
 SWO_Init.Pin = GPIO_PIN_3;
 SWO_Init.Mode = GPIO_MODE_AF_PP;
 SWO_Init.Speed = GPIO_SPEED_FREQ_HIGH;
 SWO_Init.Pull = GPIO_NOPULL;
 SWO_Init.Alternate = GPIO_AF0_JTD_TRACE;
 HAL_GPIO_Init(GPIOx, &SWO_Init);
}
/* USER CODE END 2 */

and am trying to get SWO output at 57600 baud using this configuration.

static void SWO_Init(uint32_t portBits)
{
uint32_t SWOSpeed = 57600; // default 64k baud rate
uint32_t SWOPrescaler = (HAL_RCC_GetHCLK4Freq() / SWOSpeed) + 1; // SWOSpeed in Hz, //note that CPU_CORE_FREQUENCY_HZ is expected to be the AHB4 core clock
 
 CoreDebug->DEMCR |= CoreDebug_DEMCR_TRCENA_Msk; // enable trace in core debug
 TPI->SPPR = 0x00000002; // "Selected PIN Protocol Register": Select which protocol to use for trace output (2: SWO NRZ, 1: SWO Manchester encoding)
 TPI->ACPR = SWOPrescaler;//"Async Clock Prescaler Register". Scale the baud rate of the asynchronous output
 ITM->LAR = 0xC5ACCE55; // ITM Lock Access Register, C5ACCE55 enables more write access to Control Register 0xE00 :: 0xFFC
 ITM->TCR = ITM_TCR_TraceBusID_Msk | ITM_TCR_SWOENA_Msk | ITM_TCR_SYNCENA_Msk | ITM_TCR_ITMENA_Msk; // ITM Trace Control Register
 ITM->TPR = ITM_TPR_PRIVMASK_Msk; // ITM Trace Privilege Register
 ITM->TER = portBits; // ITM Trace Enable Register. Enabled tracing on stimulus ports. One bit per stimulus port.
 
 DWT->CTRL = 0x400003FE; // DWT_CTRL bits - meaning uncertain
 TPI->FFCR = 0x00000100; // Formatter and Flush Control Register - bit 1=0 => SWO output only
}

The SWO configuration has worked on other cortex M4 cores. Does anybody have an idea what might be missing? (separate clock for TPIU FIFO?)

Thanks

This topic has been closed for replies.