Skip to main content
DOrba.1
Associate
Aug 13, 2020 5:39 AM UTC
Question

How to get FUOTA working properly on an STM32WB55RG? I am using the P-NUCLEO-WB55 board.

I have followed the workshop on https://www.youtube.com/watch?v=V_qVURNbWuM&list=PLnMKNibPkDnHCD2Xc_xX-nWR7AoWBPK2Q. And the first time I went through it everything worked fine.

However, when I tried it a second time it did not:

I loaded the BLE_Ota_x.bin to the board using the programmer. I then use the ST BLE Sensor app to upload BLE_p2pServer_ota_x.bin into the board and set the memory allocation to 0xC000. This upload works well, but then if I want to load a new code through the app, e.g. the BLE_HeartRate_ota_x.bin, it does not work.

The file does not appear as selected firmware, after tapping the SELECT FILE button and selecting the file. If instead, I tap the round button with the refresh arrow, I get a message saying "No node was found".

I tried using the dongle in transparent mode as well and get an error or no response message after trying to upload the code.

Thanks in advance.

Cheers,

Derek

This topic has been closed for replies.

4 replies

Remi QUINTIN
ST Technical Moderator
Aug 13, 2020 3:41 PM UTC

I did not check the content of the MOOC but just note that you cannot upgrade the FUS twice on a STM32WB device.

Once a version of FUS is installed on the chip, you will get error if you try to install it a second time.

This is not the case for the wireless stack.

Just check this point, avoid any new FUS installation.

Remi QUINTIN
ST Technical Moderator
Aug 13, 2020 3:55 PM UTC

Did you erase the previous ​BLE_p2pServer_ota_x.bin before loading the BLE_HeartRate_ota_x.bin?

Why using 0xC000? I use 0x7000 as start address for the OTA download. Note that it should not make a difference.

DOrba.1
DOrba.1Author
Associate
Aug 14, 2020 2:51 AM UTC

I do not erase the previous BLE_p2pServer_ota_x.bin before loading the BLE_HeartRate_ota_x.bin. In the app, I can't select a file with the "Application Coprocessor Binary" or the Custom option. When trying to upload code using the RF-Monitor, I get no response (See attached image). Regarding the previous comment, there might have been more than one attempt to upgrade the FUS, since I was not the only one working with the board.

DOrba.1
DOrba.1Author
Associate
Aug 14, 2020 3:08 AM UTC

I dragged the ble_ota_x.bin into the E: -drive and tried uploading new code using the android app. When I do this, I get an upload bar with no notification stating that the upload was completed (see attached image).