Skip to main content
YO.1
Associate II
Jan 9, 2023 4:22 AM UTC
Question

How to flash code in LoRa-E5 without using STM programmer?

Hi team, I have purchased a development kit (LoRa-E5) from Seeed website. I would like to know the method to flash the code into the controller without using STM programmer (ST-link). Is it possible to do this way?

Thanks.

This topic has been closed for replies.

1 reply

AScha.3
Super User
Jan 9, 2023 7:11 AM UTC

this module ?

https://www.seeedstudio.com/LoRa-E5-Wireless-Module-p-4745.html

Attention

1. Factory AT Firmware is programmed with RDP(Read Protection) Level 1, developers need to remove RDP first with STM32Cube Programmer. Note that regression RDP to level 0 will cause a flash memory mass to erase and the Factory AT Firmware can't be restored again.

2. The "PB13/SPI_SCK/BOOT" pin on the Wio-E5 module is just a normal GPIO, not the "BOOT0" pin of the MCU. This "PB13/SPI_SCK/BOOT" pin is used in the bootloader of the Factory AT firmware, to decide to jump to APP or stay in bootloader(for DFU). The real "BOOT0" pin doesn't pinout to the module, so developers need to be careful when developing low-power applications.

If you feel a post has answered your question, please click on " Best Answer ".