Skip to main content
ChrisLB
Associate II
Nov 17, 2020 6:59 PM UTC
Question

How to achieve low power Bluetooth advertising with STM32WB

I'm having issues getting the low power sleep to work with Bluetooth enabled on the STM32WB

Is there any guide or app note on steps needed to achieve lowest power level BLE advertising?

Basically no matter what I do - if I enable bluetooth advertising (code extracted from the iBeacon cubemx example) and enter stop2 mode, the stm32 takes about 5.5mA

If I comment out the call to aci_gap_set_discoverable(...) and then enter STOP2 mode, the board goes to ~50uA (most of that is the other hardware we have on this board)

So far, I have:

  • confirmed the main core is indeed going to sleep between bluetooth events (measuring the sleep time = advertising interval, also it's easy to see with the debugger)
  • tried "forcing" sleep with LL_C2_PWR_SetPowerMode(LL_PWR_MODE_STOP2) (my understanding is that I should not need to do this)
  • changing various #defines relating to power, dbg and sleep in the ble header files

I think I might be missing something obvious... Is there any way of seeing why the second core isn't going to sleep? My best guess is that it's a configuration thing but I'm at a loss with what else to try.

Perhaps I need to be using standby mode to force the m0 off between advertising events?

Any help would be greatly appreciated!

Thanks

This topic has been closed for replies.

16 replies

ST Employee
Nov 18, 2020 10:51 AM UTC

​Hello,

You shall never try to force the LOW power mode of CPU2 using any LL_C2_*** API and there is nothing you need to do on CPU1 side to force any CPU2 low power mode.

The CPU2 manage on its own the best low power mode to be applied and the application shall only take care of the CPU1 low power mode n the same way that you would do on any STM32 single core platform.

There are only two exceptions compare to what you would have done on a single core STM32 platform

1/ LL_C2_PWR_SetPowerMode(LL_PWR_MODE_SHUTDOWN); is called one time at startup in SystemPower_Config() to overwrite the reset value in case you plan to enter low power mode on CPU1 without starting yet CPU2.

2/ The entry/exit of low power mode ( expecially Stop Mode) need to use/check semaphores to handle synchronization with the CPU2.

These algorithm are described in AN5289 rev4 - chapter 4.3 Shared peripherals.

These algorithm are implemented in stm32_lpm_if.c.

Either you are using HSE as system clock and you should use stm32_lpm_if.c. with NO modification and call or you decide to use another system clock. In that case, you just need to update the following piece of code in stm32_lpm_if.c. - PWR_ExitStopMode() according to your need

 LL_RCC_HSE_Enable( );
 while(!LL_RCC_HSE_IsReady( ));
 LL_RCC_SetSysClkSource(LL_RCC_SYS_CLKSOURCE_HSE);
 while (LL_RCC_GetSysClkSource( ) != LL_RCC_SYS_CLKSOURCE_STATUS_HSE);

Regards.

ChrisLB
ChrisLBAuthor
Associate II
Nov 18, 2020 1:35 PM UTC

Thanks for this, really useful to get definitive answers!

I believe however I am already doing everything you describe:

1) SystemPower_Config() in app_entry.c

 LL_RCC_SetClkAfterWakeFromStop(LL_RCC_STOP_WAKEUPCLOCK_HSI);
 UTIL_LPM_Init();
 /* Initialize the CPU2 reset value before starting CPU2 with C2BOOT */
 LL_C2_PWR_SetPowerMode(LL_PWR_MODE_SHUTDOWN);

2) I have left the PWR_EnterStopMode() & PWR_ExitStopMode() unchanged (we are using HSE)

EnterStopMode (comments removed for upload):

 HAL_SuspendTick();
 while( LL_HSEM_1StepLock( HSEM, CFG_HW_RCC_SEMID ) );
 if ( ! LL_HSEM_1StepLock( HSEM, CFG_HW_ENTRY_STOP_MODE_SEMID ) )
 {
 if( LL_PWR_IsActiveFlag_C2DS( ) )
 {
 LL_HSEM_ReleaseLock( HSEM, CFG_HW_ENTRY_STOP_MODE_SEMID, 0 );
 Switch_On_HSI( );
 }
 }
 else
 {
 Switch_On_HSI( );
 }
 
 LL_HSEM_ReleaseLock( HSEM, CFG_HW_RCC_SEMID, 0 );
 
 
 LL_PWR_SetPowerMode( LL_PWR_MODE_STOP2 );
 LL_LPM_EnableDeepSleep( ); /**< Set SLEEPDEEP bit of Cortex System Control Register */
 
 __WFI();

Is there any way of seeing why the second core isnt going to sleep on its own? Maybe it's something to do with the debugger interface? I am able to attach the debugger and wake the device from sleep which I was not expecting given my configuration

ST Employee
Nov 20, 2020 5:09 PM UTC

​Hello,

As long as you are able to enter Stop Mode 2 when commenting out aci_gap_set_discoverable(), I am wondering if you just did not crash the CPU2 which would explain in some way in stays in run mode. 5.5mA means likely both CPU2 and BLE IP Core are in run mode (provided CPU1 is in sleep)

Although it burns 5.5mA, does the product works properly ?

Alternatively, I would load the p2p_server example as provided and check how much power you are measuring to make sure your tooling is fine. p2p_server is first advertising for 60s and then it stops.

In order to get some insigth of what is currently doing the CPU2 and provided you have a digital analyser, you may refer to AN5289 rev4 chapter 4.8 where it is described it is possible to monitor most real time activity on CPU2.

Everything is configured from app_debug.c.

Regards.

ChrisLB
ChrisLBAuthor
Associate II
Nov 21, 2020 11:30 AM UTC

So I've continued experimenting and changed all clock settings to match the example and added a call to APPD_init() to APPE_init() (copied from beacon example, not present in generated code) and it is now taking ~3mA and is advertising correctly.

If I comment out the aci_gap_set_discoverable now, but leave APPE_Init the processor takes about 2.7mA, which I think indicates advertising is taking roughly the amount of power I would expect, but we still have that confusing baseline consumption

I tried the p2p_server previously with no change (ie it worked but still high consumption) but will retry. I had also tried the heartrate and beacon profiles, all with same results.

The biggest clue I've found so far is that when I have CPU2 on, the debugger never detaches, despite setting DBGMCU->CR = 0 and C1 being put into stop2 mode. If I comment out all ble code (APPE_init and scheduler loop) and set C2 into shutdown mode, the debugger detaches as expected.

Not sure if any of this helps narrow down the problem. Thanks for the monitoring tip from AN5289 - I'll get hold of an analyser and see what I can do

Your point about crashing C2 seems feasible too. When experimenting, I often have to disconnect and reconnect power on the board to get advertising to work again. When "crashed", the power consumption is still the same (3mA) but no advertising occurs.

ChrisLB
ChrisLBAuthor
Associate II
Nov 18, 2020 3:52 PM UTC

Follow up thought... is it possible I'm wrong in saying that C1 is definitely asleep? I've assumed that the time spent inside _WFI() = sleep time, but maybe that's not the case? Is there anything that C2 would do that would keep C1 from sleeping? (I dont mean can c2 wake up c1- that is very clearly the case - but actually is there anything preventing sleep)

ST Employee
Nov 20, 2020 5:00 PM UTC

​Hello,

No, I do not see how C2 could prevent C1 going to sleep mode.

You may toggle GPIO before and after UTIL_LPM_EnterLowPower() in UTIL_SEQ_Idle() to check if C1 enters sleep mode. You will need a digital analyser to check the GPIOs.

Regards

ChrisLB
ChrisLBAuthor
Associate II
Nov 21, 2020 11:36 AM UTC

I'm using the RTC timer to count time in sleep mode - I think this works too? Effectively read the RTC counter before and after EnterLowPower and print the difference.

Interestingly sometimes the core wakes up at the advertising interval, sometimes using the RTC Wakup timer (5000ms) I'm using. I'm sure this comes down to my interrupt configuration (I've tried a lot of different code examples..) but as far as I can tell it does not matter (in that waking every 5s does not prevent C2 from advertising at 1000ms interval)

Mathieu Wernsen
Associate
Jun 21, 2022 3:24 PM UTC

Hi there,

@ChrisLB Did you ever manage to find a solution to this problem? I've been running into the exact same issue where calling aci_gap_set_discoverable(..) results in the CPU2 not returning to LPM when needed (i.e. after a call to aci_hal_stack_reset()). I believe this then prevents CPU1 from also entering Standby/Shutdown mode and unexpected high power consumption (5.5mA)

When not having called aci_gap_set_discoverable(), CPU2 nicely returns to Deepsleep mode (checked using PWR_EXTSCR_C2DS), after resettinng the ble stack (aci_hal_stack_reset). Measured power consumption is then 20 uA (Ok considering peripherals).

Hope you can help me out!

ChrisLB
ChrisLBAuthor
Associate II
Jun 21, 2022 4:23 PM UTC

Hi Mathieu,

Sorry this is now so long ago that I can't really give you a complete answer, but I do remember it was a bug in the chip. Something totally unrelated and many many steps to ensure everything was just right.

From what I can remember:

  • be very careful with your debugger and settings (debug sleep enable causes higher power consumption, sometimes. Sometimes with it disabled but booting up with debugger I had 0.9ma. I always power cycled with debugger disconnected before testing). You can get it to work, it's just unreliable at best (using segger Jlink plus with ozone at least)
  • ADC clock needs to be disabled in sleep. Don't ask me why..
  • make sure your calls to the sequencer are running reliably (that loop is critical to getting CPU2 to do what it's supposed to)
  • test out disabling core 2 fully. In my case sending powerdown to C2 still didnt solve my problems reliably

Essentially, I never figured out if it was actually a core 2 / bluetooth issue, or more of a total system issue. Seemed to be something with shared clock signals, but once I got it working I didnt really look back!

Mathieu Wernsen
Associate
Jun 21, 2022 4:45 PM UTC

Hi Chris,

Thanks for the quick response! Very understandable you forgot about the specifics of the final solution, but I can definitely work with your suggestions.

  • I also noticed the issues with the debugger connected and I've adopted the same workflow of flashing, disconnecting debugger + power cycling, before measuring power consumption.
  • Interesting fact. I will check this one out.
  • I'm making use of FreeRtos for this project. I was hoping the implementation provided by STM in their code generation would result in reliable task handling of the BLE stack, but I will verify this just to be sure.
  • Could you clarify this a bit? In my understanding the C2 manages it's own power state, so how could I send a powerdown command to C2? I was kind of expecting the aci_hal_stack_reset to fully shutdown C2.

I guess I just have to spend a few more hours/days fiddling around with settings, hoping to find the solution to this bug, to then hopefully never look back as well :)

ChrisLB
ChrisLBAuthor
Associate II
Jun 21, 2022 5:12 PM UTC

you might need to dig into the source code to see what stack reset does. I used the low level LL libs

LL_C2_PWR_SetPowerMode(LL_PWR_MODE_SHUTDOWN);

good luck! I hope for your sake that is is a few hours/days, not weeks like me!

ChrisLB
ChrisLBAuthor
Associate II
Jun 21, 2022 5:22 PM UTC

btw I've just rechecked our firmware.. no sign of the ADC thing (probably because we stopped using the ADC), so perhaps that was a red herring? All I know was that at the time, even with readings disabled in sleep, I had to kill the peripheral clock to signal to get it working on low power..

Mathieu Wernsen
Associate
Jun 27, 2022 7:40 AM UTC

After some further investigation I found out that for me not the ADC clock settings were the issue, but the RNG Clock setting was the cause of the CPU2 not going into Deep Sleep mode (even after a reset of the BLE stack). Switching from the LSE to the HSI48 solved my issues :)

ChrisLB
ChrisLBAuthor
Associate II
Jun 27, 2022 7:49 AM UTC

Ah nice!! Glad you got it sorted. That actually does sound familiar, I remember moving something to an internal clock also. Probably too much to ask but maybe ST will document this "feature" one day

Mathieu Wernsen
Associate
Jun 27, 2022 8:50 AM UTC

Or maybe provide an explanation so we at least understand what is happening inside this "Black-box" called CPU2.

ASett.2
Visitor II
Apr 26, 2023 3:14 PM UTC

To anyone else having an issue similar to this, I'd like to share our recent WB55 BLE advertising sleep debugging experience.

TL;DR: We changed from using hci_reset() to aci_hal_stack_reset() and it solved our power consumption problem.

We were having nearly the exact same current consumption issue when using aci_gap_set_discoverable(). Our WB55 would enter sleep mode correctly, and the M0 core would continue to advertise correctly with the expected level of power consumption, but only for a short time. Anywhere from 15 minutes to ~hours later, we would suddenly see a ~5mA current consumption increase, which would remain for hours, and sometimes resolve itself. We setup a weekend power monitoring test and saw the device enter and leave this high power state, multiple times, for hours at a time.

We tried all the suggestions in this thread and were still having the issue. After seeing references to the aci_hal_stack_reset() call here, we noticed in AN5270 it says: "This command is equivalent to HCI_RESET, but ensures that Sleep mode is entered immediately after its completion.". We had originally ruled this out as our device WOULD enter low power mode correctly at first (when using hci_reset), but the high power consumption would only occur sometime later after running.

We were desparete to try anything so we replaced our call to hci_reset() with aci_hal_stack_reset() in our init routine, ran it through our power consumption tests, and we have been running in low power mode ever since. I'm still not quite sure why hci_reset() would start out having the M0 core go into low power mode only for it to leave low power mode later, but if the functionality is really equivilant as AN5270 says, I see no reason to not use aci_hal_stack_reset() in place of hci_reset() as a general rule.