Skip to main content
IvanL
Visitor II
Jul 19, 2021 7:52 PM UTC
Question

How implement BLE client multiconnection with WB55?

Good time of day!

I am facing some problems with testing example app (BLE_p2pRoteur on WB55.Nucleo board).

First one board flashed as a client, 3 others as a servers, Server 1 to 3 are defined in app_conf.h file, corresponding appplication numbers in macros #define P2P_SERVERx are set.

When I am start scanning from the client side, it shows that 3 boards are advertising, but when connection process starts, only two boards stays connected, not 3 (see log).

The main question is: can I make simultaneous connection on STM32WB for 6 servers and how?

This topic has been closed for replies.

4 replies

Remi QUINTIN
ST Technical Moderator
Aug 13, 2021 7:53 AM UTC

BLE_p2pRouteur project is handling up to 6 connections to servers as a client and to one client as a server.

Your log does not show any trial to connect to server 3.

are you sure it does? Hard to say why the connection is not established with server 3 if the client tried to connect.

SGimm.1
Associate
Jan 18, 2022 5:12 PM UTC

Hello IvanL, Hello Remi QUINTIN

I am sadly not able to answer your question, since I have some problems bevor i even reached the mentioned problem.

Currently i am trying to implement a Client (central) on my STM32WB55RE, which should parse with a BLE from an other sensor. But i have no Idea how to accomplish this.

I was able to creat a server with the Nucleo, but this doesn't help me at the moment. Do you know any reference or tutorial on how i can implement e client?

Kind regards,

Samuel

Remi QUINTIN
ST Technical Moderator
Jan 18, 2022 5:38 PM UTC

You can have a look at the project BLE_p2pClient in the WB FW package.

SGimm.1
Associate
Jan 19, 2022 8:57 AM UTC

Thanks, I take a look