Skip to main content
JWieb
Associate III
July 18, 2019
Question

How do i use the standalone USB (CN11) for Discovery board B-L072Z-LRWAN1?

  • July 18, 2019
  • 4 replies
  • 1369 views

I am trying to use the standalone USB (CN11) for Discovery board B-L072Z-LRWAN1. But nothing seems to be happening. I have shorted the two jumper SB16 and SB15 and measured a solid 3.3v on VDD_USB_LRA and VDD_MCU_LRA. The USB lines dont seem to waiver at all from 0v.

My intent is to use the onboard bootloader (with BOOT0 HIGH) for programming.

This question was answered before but there isn't much of an answer.

https://community.st.com/s/question/0D50X00009XkWODSA3/bl072zlrwan1-cn11-usb-conn-device-mode

This topic has been closed for replies.

4 replies

Tesla DeLorean
Guru
July 19, 2019

@Community member​ has had a USB CDC running from the Murata part, I believe he used CubeMX to bring up the port.

For the system boot-loader, I'd perhaps check the OSC_IN source (SB13 ?)

Perhaps port

STM32Cube_FW_L0_V1.11.2\Projects\STM32L073Z-EVAL\Applications\USB_Device\CDC_Standalone

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
JWieb
JWiebAuthor
Associate III
July 19, 2019

I figured it out. There is another solder bridge SB37 that needs to be cut. This connects the target MCU RESET to the ST-link RESET so without powering the ST-link the reset line gets pulled low.

Why wasnt this a regular jumper?!

Thanks for the help!

xarion
Associate II
November 13, 2020

Hello @JWieb​ Just wondering what firmware you used, did it enumerate a serial port?

Tesla DeLorean
Guru
November 13, 2020

Yes, it can come up as a VCP/CDC, there isn't a stock firmware.

You'd basically have to make a generic STM32L0 CDC, perhaps look at the examples for the EVAL series boards, or have CubeMX generate some boiler-plate code, and then merge that into a LoRa project.

Figure several hours to get something clean and workable.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..