How do I send the data from my external soil moisture sensor by ADC being connected to an ADC input of the B-L072Z-LRWAN1 microcontroller using the I-CUBE-LRWAN1 example on the web or another method?
Hello everyone,
I am completely new to the forum and to the world of LoRaWAN on microcontrollers.
I am doing my undergraduate final project. This is based on a B-L072Z-LRWAN1 core that has a couple of sensors connected to it. One of them is an ADC sensor that measures the humidity of the ground.
My problem is that I would like to send the data from this sensor via LoRaWAN to TTN. In support they helped me with the existing example (I-CUBE-LRWAN) and told me that I could modify this code to do it.
I have investigated the code a bit and I have found the task of sending data by LoRa, but of course my sensor is external and I must configure the pins for an analog measurement, and not having an .ioc I can not do it through CubeMX.
Can someone help me to add my sensor and port the code to send my data.
Best regards, and thanks a million.