Skip to main content
APate.6
Associate
Jun 8, 2020 4:10 PM UTC
Question

How do I get P-NUCLEO_LRWAN2 sensor up and running via firmware update?

I cannot access the USI I-NUCLEO-LRWAN1 expansion board using serial interface hence I have to make the necessary changes in firmware and upload it to the NUCLEO-L073RZ board. I am trying to use the End Node example with the Loriot server. I made the following changes:

1) In Commissioning.h file, I set the device EUI, join/app EUI, app KEY. According to this forum post, I set the network KEY as the app KEY. I set the device address to the value given by the Loriot server when I registered the device.

2) I changed default DEFINE parameter for the frequency band to REGION_AS923.

I then uploaded the binary file generated after compiling to the baseboard using the ST-LINK UTILITY. Despite these changes, I am not able to see any data on Loriot. Am I missing anything? Any help is much appreciated!

This topic has been closed for replies.