Skip to main content
Jlim.1
Associate II
Jan 24, 2021 2:22 PM UTC
Question

How do I apply the I-CUBE-LRWAN project to the custom board?

Hello. I'm going to proceed with the Murata module project.

I downloaded the AT_SLAVE example source on the EVK LoRa® Discovery kit (B-L072Z-LRWAN1) to confirm that the data communicates well.

The binary used in the above project was downloaded to the custom board and sent the data as it did on the development board, but the data was not received on gateway.

The configuration of the custom board is connected to another stm32 mcu by the Murata module (CMWX1ZZABZ) as uart.

When the "AT+SEND=0:hello" command was sent to the lora module, i received an OK response, but no data came into the gateway.

It's a good method on the development board.

When I download the binary to Murata module on the custom board, should I download it with a different option than the one I downloaded to Murata module on the development board?

This topic has been closed for replies.

3 replies

Tesla DeLorean
Guru
Jan 24, 2021 2:44 PM UTC

The software should be the same, you'd probably want to consider differences in the external interfacing.

Perhaps the radio, and the GPIOs

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Jlim.1
Jlim.1Author
Associate II
Jan 24, 2021 3:53 PM UTC

Thank you for your answer.

I didn't understand what you meant., but please tell me in more detail.

Jlim.1
Jlim.1Author
Associate II
Jan 24, 2021 3:53 PM UTC

.​