Question
How create devEUI for public Lora network?
I have one product with inside the module Murata CMW. The product will be present on a public Lora network. The product is a sensor, so it will trasmit data
I need to go in mass production and I need to create the devEUI for each device
How I can create it?
I see there is method to create the devEUI from a MAC address (that I have avaiable), but it's deprecated
The method is use one MAC adding FF and FE on the 4th and 5th byte and turning to 1 the 7th bit of first byte.
Is there other valid method to create the devEUI witout problem?