Skip to main content
Senior
Aug 3, 2024 7:16 AM UTC
Solved

How can receive data over phone in BLE MESH

I have configured a BLE MESH with two nodes one as client and other as server . It is working well . 
I also want to recieve the same data that is being exchanged on Phone.  Can someone tell me how this can be done and what app I must use.

This topic has been closed for replies.
RiturajBest answer
Senior
Aug 10, 2024 7:07 PM UTC

To do this just flash any MESH MODEL SENSOR application to th dev  boards . in the configuration header file comment the client define and remove the slash from server model.

Turn on both the devices . Go for provsioning ,I have done this with STM32WB5MM-DK .Here is the process. Open a terminal like tera term or Hterm and then setup the port baud rate 9600 . After this click on reset and B1 together and release reset . Once you relese reset hold B1 and you will see the Blue LED blinks once it blink Check the BLE MESH APP now . On the right edge click on + and just get done with setting up both devices . Once added go into model section and then click on B1 on server and you will get tempreture on phone as well as client  hold B1 for distance . Other important parts are simply in the read me file.

3 replies

RiturajAuthor
Senior
Aug 7, 2024 9:52 AM UTC

solved

STTwo-32
ST Technical Moderator
Aug 8, 2024 3:45 PM UTC

Hello @Rituraj 

Please add your solutions. It may help someone else having same problem.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
RiturajAuthorBest answer
Senior
Aug 10, 2024 7:07 PM UTC

To do this just flash any MESH MODEL SENSOR application to th dev  boards . in the configuration header file comment the client define and remove the slash from server model.

Turn on both the devices . Go for provsioning ,I have done this with STM32WB5MM-DK .Here is the process. Open a terminal like tera term or Hterm and then setup the port baud rate 9600 . After this click on reset and B1 together and release reset . Once you relese reset hold B1 and you will see the Blue LED blinks once it blink Check the BLE MESH APP now . On the right edge click on + and just get done with setting up both devices . Once added go into model section and then click on B1 on server and you will get tempreture on phone as well as client  hold B1 for distance . Other important parts are simply in the read me file.