Question
How can I use SubGHz_Phy_PingPong project in I-CUBE-LRWAN v2.0.0?
I'm using two LRWAN NS1 with NUCLEO-L073RZ and I want to test PingPong with SubGHz_Phy_PingPong project.
Project at Project-NUCLEO-L073RZ-Applications-SubGHz_Phy-SubGHz_Phy_PingPong-STM32CubeIDE-sx1276mb1mas is right project for the device?
Do I have to connect cable with SWCLK and SWDIO pin on RHF0M003 to download the project?
LoRaWan_End_Node project is right project for LRWAN NS1 if I want to communicate with gateway again after PingPong test?