Skip to main content
Visitor II
Oct 23, 2024 5:08 AM UTC
Question

How can I increase the BLE send rate and the memory size of the protocol stack

Need to send data at high sampling rate in real time, how to configure the maximum transfer rate and large protocol stack memory to support high-speed transmission。And how to calculate the current Bluetooth transfer rate

The connection interval has been configured to 7.5ms, and a single packet can transmit up to 245 bytes from HCI

BLE_CMD_MAX_PARAM_LEN = 255

typedef __PACKED_STRUCT
{
  uint16_t Conn_Handle_To_Notify;
  uint16_t Service_Handle;
  uint16_t Char_Handle;
  uint8_t Update_Type;
  uint16_t Char_Length;
  uint16_t Value_Offset;
  uint8_t Value_Length;
  uint8_t Value[BLE_CMD_MAX_PARAM_LEN - 12];
} aci_gatt_update_char_value_ext_cp0;
 
This topic has been closed for replies.

1 reply

STTwo-32
ST Technical Moderator
Nov 19, 2024 10:04 AM UTC

Hello @jiefeng_wang 

To achieve a maximize throughput, I suggest you take a look at this application: https://github.com/stm32-hotspot/STM32WB-BLE-Basic-DataThroughput-Server. This app will help you to understand how to make it work on the best data throughput.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.