Skip to main content
Visitor II
Apr 28, 2025 4:35 AM UTC
Question

Higher Power Consumption on STM32WB5MM-DK Compared to STM32WB55 After BLE Connection

Hi everyone,

I'm working on a BLE application based on the Heart Rate Sensor sample. I have two boards:

STM32WB55 Nucleo board

STM32WB5MM-DK (Discovery kit with WB5MM module)


On the STM32WB55, everything works fine — after BLE connection, the current consumption stays below 1 mA, as expected.
However, when I run the same application on the STM32WB5MM-DK, I observe a much higher power consumption — around 10 mA after the BLE is connected.

Both builds use the same project settings, and I've made sure the low power modes are enabled properly in the application.
Is there something specific to the STM32WB5MM module or Discovery board that could be causing this increased power usage?

Things I already checked:

Same BLE connection parameters

Sleep/low-power modes enabled

No extra peripherals manually activated

Same firmware version on both boards


Any ideas on what might be causing this difference or what else I should look into?

This topic has been closed for replies.

1 reply

STTwo-32
ST Technical Moderator
May 22, 2025 10:12 AM UTC

Hello @ShafiYez 

The difference may be on the code. Are you using the same Low power modes on both of them. Could you check this video to see how you can analyze the power consumption on your boards.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.