Skip to main content
Associate
Mar 3, 2025 5:20 AM UTC
Solved

High current in stop 2 mode after BLE deactivation

Hi,

I am using a custom board based on P-NUCLEO-WB55 and started working from the example code BLE_p2pServer.

 

The board will normally be in stop2 mode and will check for pushbutton press every 1 second. The current consumption is around 10 uA in this state.

 

If push button is pressed for 3 or more seconds. The board enters the BLE mode. It is advertising the packets for a set time of 5 minutes. After 5 minutes I am exiting from the while loop. I am trying to stop the BLE mode and go to stop2 mode and continue the previous operation. 

Once i enter the BLE mode and exit out of BLE mode the current consumption is now 100uA. All other functionalities are working properly. If I press the push button for 3 seconds, The board enters BLE and starts advertising. I am trying to find out what is causing this increase in current. I don't want to reset the board every time I enter BLE mode. This is the following procedure I am using to exit out of BLE mode.

 

hci_reset();
HAL_Delay(100); 

SHCI_C2_Reinit();

LL_C2_AHB3_GRP1_DisableClock(LL_C2_AHB3_GRP1_PERIPH_IPCC);

MX_IPCC_DeInit();

HAL_NVIC_DisableIRQ(HSEM_IRQn);
__HAL_RCC_HSEM_CLK_DISABLE();

LL_C2_PWR_SetPowerMode(LL_PWR_MODE_SHUTDOWN);

and I am using this to enter stop 2 mode.

HAL_RTCEx_SetWakeUpTimer_IT(&hrtc, SLEEP_MODE_DURATION, RTC_WAKEUPCLOCK_RTCCLK_DIV16);
HAL_SuspendTick();


/* Enter STOP 2 mode */
HAL_PWREx_EnterSTOP2Mode(PWR_STOPENTRY_WFI);
/* ... Stop 2 mode ... */


/* Resume SysTick */
HAL_ResumeTick();

 

Is my procedure correct and do I have to set any values differently to achieve the 10 uA current in my normal operating mode. Please help me to resolve this issue

 

This topic has been closed for replies.
Sarra.SBest answer
ST Employee
Mar 7, 2025 9:09 AM UTC

Hello @Jeremiah, 

Are you sure that all BLE-related peripherals and clocks are properly disabled before entering Stop 2 mode?

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

2 replies

Sarra.SBest answer
ST Employee
Mar 7, 2025 9:09 AM UTC

Hello @Jeremiah, 

Are you sure that all BLE-related peripherals and clocks are properly disabled before entering Stop 2 mode?

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
JeremiahAuthor
Associate
May 7, 2025 5:42 AM UTC

Some GPIO pins have changed their state after exiting  BLE mode and reinitialising the GPIO pins reduced the current.