Skip to main content
Associate
Jul 1, 2025 11:03 AM UTC
Solved

High Current Consumption in STOP1 Mode on STM32WB – Despite Peripheral Shutdown

Hi everyone,
I’m working with the NUCLEO - WB15CC board and I’m trying to enter STOP1 mode to minimize current consumption. However, despite disabling all unnecessary peripherals, the power consumption remains unexpectedly high (much higher than in the PWR_STOP1 example provided by STM32Cube, which works fine on the same board).

What I’ve tried so far:

  • Called HAL_SuspendTick() before entering STOP mode and HAL_ResumeTick() after wakeup

  • Called hci_reset() to reset the BLE stack

  • Configured all GPIOs as analog with no pull (using GPIO_AllAnalog())

  • Disabled clocks for all unused peripherals:

     __HAL_RCC_IPCC_CLK_DISABLE();
    __HAL_RCC_HSEM_CLK_DISABLE();
    __HAL_RCC_ADC_CLK_DISABLE();
    __HAL_RCC_LPTIM1_CLK_DISABLE();
    __HAL_RCC_LPTIM2_CLK_DISABLE();
    __HAL_RCC_TIM1_CLK_DISABLE();
    __HAL_RCC_TIM2_CLK_DISABLE();
  • Disabled all interrupts using __disable_irq() and cleared pending IRQs (RTC, IPCC, etc.)
  • Set both cores (CPU1 and CPU2) to STOP1 using:
    • LL_C2_PWR_SetPowerMode(LL_PWR_MODE_SHUTDOWN);
      LL_PWR_SetPowerMode(LL_PWR_MODE_STOP1);
      LL_LPM_EnableDeepSleep();
      __WFI();

Despite all of this, I’m still seeing much higher current than expected. Strangely, if I flash the official PWR_STOP1 example from STM32Cube, it works perfectly and the consumption is very low (100 uA).

Also if I set LL_PWR_MODE_STANDBY the consuption is low indeed, but it is ok for me stop mode that should be around 100-200 uA. However using an amperometer I reach 3mA...

My question:

What could be preventing STOP1 mode from reducing the current properly in my application, even though all peripherals and interrupts seem to be handled correctly? Are there hidden wake-up sources or configuration steps I might be missing?

Any insights would be highly appreciated!

This topic has been closed for replies.
Marco99Best answer
Associate
Jul 2, 2025 10:40 AM UTC

Thanks to everyone for the support. I finally managed to significantly reduce the power consumption in STOP1 mode.

The issue was that, even though I thought all unused peripherals were disabled, some GPIO ports and timers were still consuming current. After manually disabling specific GPIO ports and turning off timers like TIM1 and TIM2 (usingHAL_TIM_Base_DeInit and HAL_GPIO_DeInit) , the current dropped to about 18 µA, which is in line with expectations for STOP1 mode

11 replies

Andrew Neil
Super User
Jul 1, 2025 11:23 AM UTC

Welcome to the forum.

Please see How to write your question to maximize your chances to find a solution for best results; in particular:

  • What board are you using? If a custom board, show schematics.
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Marco99Author
Associate
Jul 1, 2025 12:30 PM UTC

Yes sorry,  I updated the post

Andrew Neil
Super User
Jul 1, 2025 1:28 PM UTC

When measuring consumption, you need to

  • Ensure ST-Link is disconnected
  • Do a power cycle (not just a reset) after using the debugger
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
FilipKremen
ST Employee
Jul 2, 2025 8:02 AM UTC

Hello,

it's not necessary to implement entering stop mode since the BLE examples include low power manager. The MCU enters low power mode automatically when there is no pending task in the sequencer.

 

Best regards,

Filip Kremen

Marco99AuthorBest answer
Associate
Jul 2, 2025 10:40 AM UTC

Thanks to everyone for the support. I finally managed to significantly reduce the power consumption in STOP1 mode.

The issue was that, even though I thought all unused peripherals were disabled, some GPIO ports and timers were still consuming current. After manually disabling specific GPIO ports and turning off timers like TIM1 and TIM2 (usingHAL_TIM_Base_DeInit and HAL_GPIO_DeInit) , the current dropped to about 18 µA, which is in line with expectations for STOP1 mode