Skip to main content
apm
Associate
Mar 19, 2023 8:40 PM UTC
Question

Hi, I want to port the LoRaWAN software expansion for STM32Cube to a STM32L071CBT connected to a SX1276 chip. I don't know where to start. Can someone please explain the steps to take to port this LoRawan library?

..

This topic has been closed for replies.

4 replies

Tesla DeLorean
Guru
Mar 19, 2023 9:17 PM UTC

That's going to be very similar to the Murata module in the B-LRWAN1 Discovery board

​

​Watch for pin usage differences.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
apm
apmAuthor
Associate
Mar 25, 2023 4:38 PM UTC

Hi,

Thank you for the answer. The Murata module is based on the STM32L072CZ so must I create a new project for the STM32L071CBT in CubeIDE and create the right pin connections and other peripheral configurations (like CubeMX) and than copy de code from de Murata module (B-LRWAN1) in the new project? Or can I change the existing B-LRWAN1 code in the LoRaWAN software expansion?

Tesla DeLorean
Guru
Mar 25, 2023 9:07 PM UTC

I'm using Keil, I'd dupe the project and change the target..

I don't like the code generators, so I'd start with something that works (hw+sw), get the lay of the land from that, and then pivot into what I'm trying to port on to. I've moved the earlier LRWAN code onto F1, L4 and F7 etc.

With Radio it's very helpful to have something that Works, because it helps isolate receiver and transmit issues on the new platform. It's very difficult to debug if nothing you have is known to function properly.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
apm
apmAuthor
Associate
Mar 26, 2023 8:23 AM UTC

Thanks again for the explanation. I will follow your advice and use the B-LRWAN1 code as start for my STM32L071CBT code. I also installed Keil and will give it a try.

Regards