Skip to main content
WNowa.1
Associate
Oct 30, 2020 5:10 PM UTC
Question

Hi, i'm doing a code in C for stm32 with LoRa-02, and i came across a weird error.

Hi, i'm doing a code in C for stm32 with LoRa-02, and i came across a weird error.

error:

expected declaration specifiers or '...' before '(' token

A part of a code:

0693W0000059vOcQAI.png 

txt:

define PERIPH_BASE (0x40000000UL) /*!< Peripheral base address in the alias region */
 
 
/*!< Peripheral memory map */
#define APBPERIPH_BASE PERIPH_BASE
#define AHBPERIPH_BASE (PERIPH_BASE + 0x00020000UL)
#define IOPPERIPH_BASE (PERIPH_BASE + 0x10000000UL)

I'm useing a sts library for SX1278. I don't understand whats wrong with the definition. It seems like the declaration sequence is done correctly, maybe something with nested definitions or something, i don't know. Also when i copypaste this fragment of code into new project, error disapears.

Sorry for my bad london, thx for help :v

edit 1: deleted

edit 2:

My code (main.c) is just a few #include and an endless loop.

Part of a code where PERIPH_BASE is used. It's hal rcc header file:

/* Disable Backup domain write protection state change timeout */
#define RCC_DBP_TIMEOUT_VALUE (100U) /* 100 ms */
/* LSE state change timeout */
#define RCC_LSE_TIMEOUT_VALUE LSE_STARTUP_TIMEOUT
#define CLOCKSWITCH_TIMEOUT_VALUE (5000U) /* 5 s */
#define HSE_TIMEOUT_VALUE HSE_STARTUP_TIMEOUT
#define MSI_TIMEOUT_VALUE (2U) /* 2 ms (minimum Tick + 1) */
#define HSI_TIMEOUT_VALUE (2U) /* 2 ms (minimum Tick + 1) */
#define LSI_TIMEOUT_VALUE (2U) /* 2 ms (minimum Tick + 1) */
#define PLL_TIMEOUT_VALUE (2U) /* 2 ms (minimum Tick + 1) */
#if defined(RCC_HSI48_SUPPORT)
#define HSI48_TIMEOUT_VALUE (2U) /* 2 ms (minimum Tick + 1) */
#endif /* RCC_HSI48_SUPPORT */
/**
 * @}
 */
 
 
/** @defgroup RCC_BitAddress_AliasRegion BitAddress AliasRegion
 * @brief RCC registers bit address in the alias region
 * @{
 */
#define RCC_OFFSET (RCC_BASE - PERIPH_BASE)
/* --- CR Register ---*/
/* Alias word address of HSION bit */
#define RCC_CR_OFFSET (RCC_OFFSET + 0x00U)
/* --- CFGR Register ---*/
/* Alias word address of I2SSRC bit */
#define RCC_CFGR_OFFSET (RCC_OFFSET + 0x08U)
/* --- CSR Register ---*/
#define RCC_CSR_OFFSET (RCC_OFFSET + 0x74U)
 
/* CR register byte 3 (Bits[23:16]) base address */
#define RCC_CR_BYTE2_ADDRESS (0x40023802U)
 
/* CIER register byte 0 (Bits[0:8]) base address */
#define CIER_BYTE0_ADDRESS ((uint32_t)(RCC_BASE + 0x10U + 0x00U))
/**

 edit 3:

C:/Users/Wojtek/workspace/RA_B-L072Z-LRWAN1/inc/mlm32l0xx_hw_conf.h:120:42: note: in expansion of macro 'USART2'
 #define USARTx USART2
 ^~~~~~
C:/Users/Wojtek/workspace/RA_B-L072Z-LRWAN1/HAL_Driver/Inc/stm32l0xx_ll_rcc.h:1586:62: note: in expansion of macro 'USARTx'
 __STATIC_INLINE uint32_t LL_RCC_GetUSARTClockSource(uint32_t USARTx)

,,In your declaration of function LL_RCC_GetUSARTClockSource, you have attempted to give the parameter a name (USARTx) that is already defined as a macro identifier. The result is that the parameter / macro name is replaced with the macro's expansion text, which ultimately draws on your PERIPH_BASE macro. That's not valid at that point."

This /\ is a comment from the stackoverflow forum, thanks to some random community member for finding this.

the function that probably cause the problem:

stm32l0xx_ll_rcc.c:

uint32_t LL_RCC_GetUSARTClockFreq(uint32_t USARTxSource)
{
 uint32_t usart_frequency = LL_RCC_PERIPH_FREQUENCY_NO;
 
 /* Check parameter */
 assert_param(IS_LL_RCC_USART_CLKSOURCE(USARTxSource));
#if defined(RCC_CCIPR_USART1SEL)
 if (USARTxSource == LL_RCC_USART1_CLKSOURCE)
 {
 /* USART1CLK clock frequency */
 switch (LL_RCC_GetUSARTClockSource(USARTxSource))
 {
 case LL_RCC_USART1_CLKSOURCE_SYSCLK: /* USART1 Clock is System Clock */
 usart_frequency = RCC_GetSystemClockFreq();
 break;
 
 case LL_RCC_USART1_CLKSOURCE_HSI: /* USART1 Clock is HSI Osc. */
 if (LL_RCC_HSI_IsReady() != 0U)
 {
 if (LL_RCC_IsActiveFlag_HSIDIV() != 0U)
 {
 usart_frequency = (HSI_VALUE >> 2U);
 }
 else
 {
 usart_frequency = HSI_VALUE;
 }
 }
 break;
 
 case LL_RCC_USART1_CLKSOURCE_LSE: /* USART1 Clock is LSE Osc. */
 if (LL_RCC_LSE_IsReady() != 0U)
 {
 usart_frequency = LSE_VALUE;
 }
 break;
 
 case LL_RCC_USART1_CLKSOURCE_PCLK2: /* USART1 Clock is PCLK2 */
 default:
 usart_frequency = RCC_GetPCLK2ClockFreq(RCC_GetHCLKClockFreq(RCC_GetSystemClockFreq()));
 break;
 }
 }
#endif /* RCC_CCIPR_USART1SEL */
 
#if defined(RCC_CCIPR_USART2SEL)
 if (USARTxSource == LL_RCC_USART2_CLKSOURCE)
 {
 /* USART2CLK clock frequency */
 switch (LL_RCC_GetUSARTClockSource(USARTxSource))
 {
 case LL_RCC_USART2_CLKSOURCE_SYSCLK: /* USART2 Clock is System Clock */
 usart_frequency = RCC_GetSystemClockFreq();
 break;
 
 case LL_RCC_USART2_CLKSOURCE_HSI: /* USART2 Clock is HSI Osc. */
 if (LL_RCC_HSI_IsReady() != 0U)
 {
 if (LL_RCC_IsActiveFlag_HSIDIV() != 0U)
 {
 usart_frequency = (HSI_VALUE >> 2U);
 }
 else
 {
 usart_frequency = HSI_VALUE;
 }
 }
 break;
 
 case LL_RCC_USART2_CLKSOURCE_LSE: /* USART2 Clock is LSE Osc. */
 if (LL_RCC_LSE_IsReady() != 0U)
 {
 usart_frequency = LSE_VALUE;
 }
 break;
 
 case LL_RCC_USART2_CLKSOURCE_PCLK1: /* USART2 Clock is PCLK1 */
 default:
 usart_frequency = RCC_GetPCLK1ClockFreq(RCC_GetHCLKClockFreq(RCC_GetSystemClockFreq()));
 break;
 }
 }
#endif /* RCC_CCIPR_USART2SEL */
 
 return usart_frequency;
}

stm32l0xx_ll_rcc.h:

/**
 * @brief Get USARTx clock source
 * @rmtoll CCIPR USARTxSEL LL_RCC_GetUSARTClockSource
 * @param USARTx This parameter can be one of the following values:
 * @arg @ref LL_RCC_USART1_CLKSOURCE (*)
 * @arg @ref LL_RCC_USART2_CLKSOURCE
 * @retval Returned value can be one of the following values:
 * @arg @ref LL_RCC_USART1_CLKSOURCE_PCLK2 (*)
 * @arg @ref LL_RCC_USART1_CLKSOURCE_SYSCLK (*)
 * @arg @ref LL_RCC_USART1_CLKSOURCE_HSI (*)
 * @arg @ref LL_RCC_USART1_CLKSOURCE_LSE (*)
 * @arg @ref LL_RCC_USART2_CLKSOURCE_PCLK1
 * @arg @ref LL_RCC_USART2_CLKSOURCE_SYSCLK
 * @arg @ref LL_RCC_USART2_CLKSOURCE_HSI
 * @arg @ref LL_RCC_USART2_CLKSOURCE_LSE
 *
 * (*) value not defined in all devices.
 */
__STATIC_INLINE uint32_t LL_RCC_GetUSARTClockSource(uint32_t USARTx)
{
 return (uint32_t)(READ_BIT(RCC->CCIPR, USARTx) | (USARTx << 16U));
}

This topic has been closed for replies.

7 replies

TDK
Oct 30, 2020 5:59 PM UTC

Doesn't seem like an error to me. It could be caused by something else above it.

It could also be an incorrect or stale message left over from a previous build attempt. Try to clean and rebuild the project.

"If you feel a post has answered your question, please click ""Accept as Solution""."
WNowa.1
WNowa.1Author
Associate
Oct 30, 2020 6:05 PM UTC

I added a code before the error line.

Already tried to clean and rebuild the project, but it can't finish builing, cuz of this error :\ .

TDK
Oct 31, 2020 1:22 AM UTC

I have to imagine the problem is not in the definition of PERIPH_BASE, but in its usage somewhere within the code.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Tesla DeLorean
Guru
Oct 31, 2020 1:38 AM UTC

You have some mismatched brace / compound statement or #ifdef/#endif type construct somewhere.

Or an errant preprocessor define.

Problem not in the library code. In YOUR code somewhere, go back to when it was working properly and work through the changes you made.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
WNowa.1
WNowa.1Author
Associate
Oct 31, 2020 1:41 PM UTC

my code is just an infinite loop :v