Skip to main content
JGhaz.1
Associate
May 16, 2022 11:05 AM UTC
Question

help with porting files from STM32F429ZI project to STM32WBRG55

this error showed when i build the project

```

c:\st\stm32cubeide_1.8.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.9-2020-q2-update.win32_2.0.0.202105311346\tools\arm-none-eabi\bin\ld.exe: C:\Users\gjallouli\STM32CubeIDE\ETO\ETO_FW_Production_Pack\Core\Src\dwt_uwb_driver\lib\libdwt_uwb_driver-hfp-5.8.0.a(deca_compat.c.obj): in function `dwt_probe':

deca_compat.c:(.text.dwt_probe+0x94): undefined reference to `__dw_drivers_start'

c:\st\stm32cubeide_1.8.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.9-2020-q2-update.win32_2.0.0.202105311346\tools\arm-none-eabi\bin\ld.exe: deca_compat.c:(.text.dwt_probe+0x98): undefined reference to `__dw_drivers_end'

```

when i searched the '__dw_drivers_start' only exists in the flash of F4 .

can i modify the flash of WB and create other sections

This topic has been closed for replies.

2 replies

Markus GIRDLAND
ST Employee
May 18, 2022 6:57 AM UTC

Yes, you can create sections as you please in the linker script of the WB.

Is this symbol supposed to be defined in the linker script or in the a library or in c code?

JGhaz.1
JGhaz.1Author
Associate
May 18, 2022 9:23 AM UTC

it's supposed to be defined in the linker script