Skip to main content
ICMosquera
Associate III
Aug 2, 2023 9:44 AM UTC
Question

HeartRate with FreeRTOS

Hi Madam/Sir,

I'd like to ask for help regarding creating a new Project replicating the HeartrateFreeRTOS example. When I load my custom board with the HeartRateFreeRTOS example, I'm able to connect with ST's BLE toolbox and see all the data incoming. So I tried to create a new project, I enable the Free RTOS and the BLE too. Unfortunately, I was only able to use the BT Sig Heart Rate Sensor profile. I compiled it and load it on the Board without touching any code. Unfortunately, I cannot detect the board on my phone.

Now here is my Question, did I miss some configuration that causes my board not to be able to be detected? I was pretty sure my board is working because I have tried the HeartRateFreeRTOS example and also tried my previous custom program received from the phone which was derived from a youtube workshop and it works.

 

Any help would be appreciated. 

 

Thanks,

Ian

This topic has been closed for replies.

1 reply

Associate III
May 22, 2024 3:18 PM UTC

Any news on this subject ? I'm trying to do the same.