Skip to main content
sebachm94
Associate
Oct 11, 2022 1:47 PM UTC
Question

HCI_LE_TEST_END long response (BLE_TransparentMode - STM32WB55)

Hi, I'm trying to run BLE_TransparentMode on my STM32WB55VG for DTM purposes. I'm using FUS 1.2.0, Wireless Stack 1.13.2 (stm32wb5x_BLE_HCILayer_extended_fw), BLE_TransparentMode app 1.13.2.

I'm building it in STM32CubeIde 1.8.0 with CubeMX 6.4.0, only thing I'm changing comparing to default config is USART-TX pin from PB7 to PA9 (in .ioc file).

App works almost fine. It responds for most of the commands with Command Complete but there is a problem while ending TX test.

HCI_LE_TRANSMITTER_TEST is sent and I got Command Complete as a result, then I'm trying to send HCI_LE_TEST_END and here is the problem. Response goes back after ~30sec, with Command Complete as result. The same app works fine for my Nucleo Board with STM32WB55 (with the same stack and FUS).

Can you help me figure it out what I could do wrong or where to debug?

BR,

Sebastian

This topic has been closed for replies.

2 replies

Remy ISSALYS
ST Technical Moderator
Nov 7, 2022 10:46 AM UTC

Hello,

Can you retry with the latest STM32CubeWB firmware package (v1.14.1), to see if you have the same issue?

Best Regards

Associate
Sep 28, 2023 12:40 PM UTC

We use BlueNRG-M2SP module on our device. To be honest, I don't really understand your answer.