Skip to main content
Associate
Nov 15, 2024 2:40 PM UTC
Solved

Having issues with STM32WL Nucleo-64. Device is not using antenna

Hi, i have started testing the STM32WL Nucleo-64 with the Lorawan End Node Firmware. At first it seem to run OK, the device connects to the gateway and the data packets reach the platform i use. But the device stops working correctly with a few mwters of distance. I have seen that the BGS13S4N9 chip is not being powered, and the signals FE_CTRL1, FE_CTRL2 and FE_CTRL3 are always on reset state, though the firmware is setting them on.I have not modify the pinout or any configuration not needed. Is this a firmware configuration issue?

 

Kind Regards,

LuisL 

This topic has been closed for replies.
LuisLBest answer
Associate
Nov 29, 2024 11:57 AM UTC

Hi i have found the problem, i had the FE_CTRL pins not configured in stm32wlxx_nucleo_radio.h and stm32wlxx_nucleo_radio.c , now it works as intended

2 replies

STTwo-32
ST Technical Moderator
Nov 25, 2024 8:59 AM UTC

Hello @LuisL 

I'm not able to reproduce this behavior. Could you try the same test using another NUCLEO-WL55JCx and see if you see the same behavior.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
LuisLAuthorBest answer
Associate
Nov 29, 2024 11:57 AM UTC

Hi i have found the problem, i had the FE_CTRL pins not configured in stm32wlxx_nucleo_radio.h and stm32wlxx_nucleo_radio.c , now it works as intended