Getting RTC value
Hello, I am reading ADC data with b-l072z-lrwan1 and send another kit. I need to add this datas to timestamp for compare different sensor datas. So I am trying to read RTC time value. I have called this function from "hw_rtc.c" ;
uint32_t CalendarValue1 = HW_RTC_GetTimerValue();code to my main loop and read RTC timer in ticks. I am reading numbers like;
[17:31:44:155] 1732371278 �?�
[17:31:44:155] 1732371279 �?�
[17:31:44:155] 1732371281 �?�
[17:31:44:155] 1732371282 �?�
[17:31:44:155] 1732371284 �?�
[17:31:44:155] 1732371285 �?�
[17:31:44:161] 1732371286 �?�
[17:31:44:161] 1732371288 �?�
[17:31:44:161] 1732371289 �?�
[17:31:44:161] 1732371291 �?�
[17:31:44:163] 1732371292 �?�
[17:31:44:163] 1732371294 �?�
[17:31:44:166] 1732371295 �?�
[17:31:44:170] 1732371296 �?�
[17:31:44:170] 1732371298 �?�
[17:31:44:170] 1732371299 �?�
[17:31:44:172] 1732371301 �?�
[17:31:44:172] 1732371302 �?�
[17:31:44:173] 1732371303 �?�
[17:31:44:175] 1732371305 �?�
[17:31:44:177] 1732371306 �?�
[17:31:44:177] 1732371308 �?�
[17:31:44:178] 1732371309 �?�
[17:31:44:181] 1732371311 �?�
[17:31:44:181] 1732371312 �?�
[17:31:44:183] 1732371313 �?�
[17:31:44:184] 1732371315 �?�
[17:31:44:185] 1732371316 �?�
[17:31:44:188] 1732371318 �?�
[17:31:44:188] 1732371319 �?�
[17:31:44:189] 1732371320 �?�
[17:31:44:191] 1732371322 �?�
[17:31:44:192] 1732371323 �?�
[17:31:44:195] 1732371325 �?�
[17:31:44:195] 1732371326 �?�
[17:31:44:198] 1732371328 �?�
[17:31:44:198] 1732371329 �?�
[17:31:44:200] 1732371330 �?�
[17:31:44:202] 1732371332 �?�
[17:31:44:202] 1732371333 �?�
[17:31:44:203] 1732371335 �?�
[17:31:44:205] 1732371336 �?�
[17:31:44:206] 1732371337 �?�
[17:31:44:207] 1732371339 �?�
[17:31:44:209] 1732371340 �?�
[17:31:44:210] 1732371342 �?�
[17:31:44:212] 1732371343 �?�
[17:31:44:213] 1732371345 �?�
[17:31:44:214] 1732371346 �?�
[17:31:44:216] 1732371347 �?�
[17:31:44:217] 1732371349 �?�
[17:31:44:220] 1732371350 �?�
[17:31:44:220] 1732371352 �?�
[17:31:44:221] 1732371353 �?�
[17:31:44:224] 1732371354 �?�
[17:31:44:227] 1732371356 �?�
[17:31:44:227] 1732371357 �?�
[17:31:44:229] 1732371359 �?�
[17:31:44:229] 1732371360 �?�
[17:31:44:231] 1732371362 �?�
[17:31:44:231] 1732371363 �?�
[17:31:44:233] 1732371364 �?�
[17:31:44:235] 1732371366 �?�
[17:31:44:235] 1732371367 �?�
[17:31:44:237] 1732371369 �?�
[17:31:44:238] 1732371370 �?�
[17:31:44:240] 1732371371 �?�
[17:31:44:241] 1732371373 �?�
[17:31:44:244] 1732371374 �?�
[17:31:44:244] 1732371376 �?�
[17:31:44:246] 1732371377 �?�
[17:31:44:246] 1732371379 �?�
[17:31:44:248] 1732371380 �?�
[17:31:44:250] 1732371381 �?�
[17:31:44:251] 1732371383 �?�
[17:31:44:253] 1732371384 �?�
[17:31:44:253] 1732371386 �?�
[17:31:44:255] 1732371387 �?�
[17:31:44:257] 1732371388 �?�
[17:31:44:258] 1732371390 �?�
[17:31:44:261] 1732371391 �?�
[17:31:44:261] 1732371393 �?�
[17:31:44:264] 1732371394 �?�
[17:31:44:264] 1732371396 �?�
[17:31:44:265] 1732371397 �?�
[17:31:44:267] 1732371398 �?�
[17:31:44:267] 1732371400 �?�
[17:31:44:268] 1732371401 �?�
[17:31:44:270] 1732371403 �?�
[17:31:44:272] 1732371404 �?�
[17:31:44:272] 1732371405 �?�
[17:31:44:275] 1732371407 �?�
[17:31:44:277] 1732371408 �?�
[17:31:44:278] 1732371410 �?�
[17:31:44:278] 1732371411 �?�Time values come from CuteCom, calendarValues like 1732....... Then i converted this value to normal date but it is wrong when i compare with RTC registers.
/*!
* @brief Get the RTC timer value
* @param none
* @retval RTC Timer value in ticks
*/
uint32_t HW_RTC_GetTimerValue( void )
{
RTC_TimeTypeDef RTC_TimeStruct;
RTC_DateTypeDef RTC_DateStruct;
uint32_t CalendarValue = (uint32_t) HW_RTC_GetCalendarValue(&RTC_DateStruct, &RTC_TimeStruct );
return( CalendarValue );
}/*!
* @brief get current time from calendar in ticks
* @param pointer to RTC_DateStruct
* @param pointer to RTC_TimeStruct
* @retval time in ticks
*/
static TimerTime_t HW_RTC_GetCalendarValue( RTC_DateTypeDef* RTC_DateStruct, RTC_TimeTypeDef* RTC_TimeStruct )
{
TimerTime_t calendarValue = 0;
uint32_t i = 0;
uint32_t first_read;
/* Get Time and Date*/
HAL_RTC_GetTime( &RtcHandle, RTC_TimeStruct, RTC_FORMAT_BIN );
/* make sure it is correct due to asynchronus nature of RTC*/
do {
// first_read = RTC_TimeStruct->SubSeconds;
first_read = RTC->SSR;
HAL_RTC_GetDate( &RtcHandle, RTC_DateStruct, RTC_FORMAT_BIN );
HAL_RTC_GetTime( &RtcHandle, RTC_TimeStruct, RTC_FORMAT_BIN );
}while( first_read != RTC->SSR );
// } while (first_read != RTC_TimeStruct->SubSeconds);
/* years (calc valid up to year 2099)*/
for( i = 0; i < RTC_DateStruct->Year; i++ )
{
if( (i % 4) == 0 )
{
calendarValue += DaysInLeapYear * SecondsInDay;
}
else
{
calendarValue += DaysInYear * SecondsInDay;
}
}
/* months (calc valid up to year 2099)*/
if(( (RTC_DateStruct->Year % 4) == 0 ) )
{
for( i = 0; i < ( RTC_DateStruct->Month - 1 ); i++ )
{
calendarValue += DaysInMonthLeapYear[i] * SecondsInDay;
}
}
else
{
for( i = 0; i < ( RTC_DateStruct->Month - 1 ); i++ )
{
calendarValue += DaysInMonth[i] * SecondsInDay;
}
}
/* days */
calendarValue += ( ( uint32_t )RTC_TimeStruct->Seconds +
( ( uint32_t )RTC_TimeStruct->Minutes * SecondsInMinute ) +
( ( uint32_t )RTC_TimeStruct->Hours * SecondsInHour ) +
( ( uint32_t )( RTC_DateStruct->Date * SecondsInDay ) ) );
calendarValue = (calendarValue<<N_PREDIV_S) + ( PREDIV_S - RTC_TimeStruct->SubSeconds);
return( calendarValue );
}What is the wrong with this. I am just call a function from library. Actually, when the first time i think to just read time registers registers as RTC_TimeStruct->Seconds, RTC_TimeStruct->Minutes, RTC_TimeStruct->Hours, but i can not solve it.Thanks for help.