Hello @Davide Dalfra
I've tested using the STM32CubeProgrammer V2.19.0 and the NUCLEO-WB09KE. I've set the JP1 of the MB2032 to bootloader mode, connected the board throw the STM32CubeProgrammer, set the connection parameters as follow (with no parity):

Finally, click on connect and on the HW reset button of the board. Everything works fine for me:
16:30:03:448 : UR connection mode is defined with the HWrst reset mode
16:30:03:452 : RTS low
16:30:03:453 : DTR low
16:30:03:462 : Serial Port COM29 is successfully opened.
16:30:03:462 : Port configuration: parity = none, baudrate = 115200, data-bit = 8, stop-bit = 1.0, flow-control = off
16:30:03:463 : No Init bits value is : 0
16:30:03:463 : Sending init command:
16:30:03:463 : #byte 0x7F sent successfully to target
16:30:07:463 : Wait ends after 2 loop, dataready = 0, delay = 4000
16:30:07:465 : Timeout error occured while waiting for acknowledgement.
16:30:07:465 : No response from target received
16:30:07:465 : Retrying UART init connection...
16:30:07:466 : #byte 0x7F sent successfully to target
16:30:07:468 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:07:468 : #ack Received response from target: 0x79
16:30:07:468 : Activating device: OK
16:30:07:469 : Board : --
16:30:07:469 : Sending GetID command and its XOR:
16:30:07:469 : #byte 0x02 sent successfully to target
16:30:07:469 : #byte 0xFD sent successfully to target
16:30:07:471 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:07:471 : #ack Received response from target: 0x79
16:30:07:472 : Received 4 data bytes from target : 0x03000106
16:30:07:472 : Chip ID: 0x32
16:30:07:472 : Sending Get command and its XOR:
16:30:07:473 : #byte 0x00 sent successfully to target
16:30:07:473 : #byte 0xFF sent successfully to target
16:30:07:473 : #ack Received response from target: 0x79
16:30:07:475 : Received 3 data bytes from target : 0x790901
16:30:07:475 : size of bytes in the response: 9
16:30:07:476 : Received 9 data bytes from target
16:30:07:477 : Full received response: 790901000102112131438292
16:30:07:477 : BootLoader protocol version: 1.0
16:30:07:477 : #byte 0x11 sent successfully to target
16:30:07:478 : #byte 0xEE sent successfully to target
16:30:07:570 : #data sent successfully to target: 0x1004000014
16:30:07:570 : #byte 0x00 sent successfully to target
16:30:07:571 : #byte 0xFF sent successfully to target
16:30:07:573 : Sending GetID command and its XOR:
16:30:07:573 : #byte 0x02 sent successfully to target
16:30:07:573 : #byte 0xFD sent successfully to target
16:30:07:573 : #ack Received response from target: 0x00
16:30:07:575 : Received 5 data bytes from target : 0x7903000106
16:30:07:579 : #byte 0x11 sent successfully to target
16:30:07:580 : #byte 0xEE sent successfully to target
16:30:07:679 : #data sent successfully to target: 0x1004000014
16:30:07:679 : #byte 0x00 sent successfully to target
16:30:07:682 : #byte 0xFF sent successfully to target
16:30:07:685 : Sending GetID command and its XOR:
16:30:07:685 : #byte 0x02 sent successfully to target
16:30:07:685 : #byte 0xFD sent successfully to target
16:30:07:685 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:07:685 : #ack Received response from target: 0x79
16:30:07:687 : Received 5 data bytes from target : 0x030001061f
16:30:09:894 : Sending GetID command and its XOR:
16:30:09:894 : #byte 0x02 sent successfully to target
16:30:09:894 : bytesToWrite before send = 1
16:30:09:894 : bFlushRet = 1, bytesToWrite after flush() = 1
16:30:09:894 : waitForBytesWritten Error : The wait operation timed out.
16:30:09:894 : #byte 0xFD sent successfully to target
16:30:09:895 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:09:895 : #ack Received response from target: 0x79
16:30:09:895 : Received 5 data bytes from target : 0x030001061f
16:30:09:895 : UPLOADING OPTION BYTES DATA ...
16:30:09:896 : Bank : 0x00
16:30:09:896 : Address : 0x10040000
16:30:09:896 : Size : 16 Bytes
16:30:09:896 : Sending Read command and its XOR:
16:30:09:896 : #byte 0x11 sent successfully to target
16:30:09:897 : #byte 0xEE sent successfully to target
16:30:09:897 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:09:897 : #ack Received response from target: 0x79
16:30:09:899 : Sending Read address and its checksum:
16:30:09:899 : #data sent successfully to target: 0x1004000014
16:30:09:899 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:09:899 : #ack Received response from target: 0x79
16:30:09:900 : Sending number of bytes to be read - 1 and its checksum:
16:30:09:900 : #data sent successfully to target: 0x0ff0
16:30:09:900 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:09:900 : #ack Received response from target: 0x79
16:30:09:900 : Received 16 data bytes from target
16:30:09:902 : UPLOADING OPTION BYTES DATA ...
16:30:09:902 : Bank : 0x00
16:30:09:902 : Address : 0x10040000
16:30:09:902 : Size : 16 Bytes
16:30:09:902 : Sending Read command and its XOR:
16:30:09:902 : #byte 0x11 sent successfully to target
16:30:09:903 : #byte 0xEE sent successfully to target
16:30:09:903 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:09:903 : #ack Received response from target: 0x79
16:30:09:903 : Sending Read address and its checksum:
16:30:09:903 : #data sent successfully to target: 0x1004000014
16:30:09:903 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:09:903 : #ack Received response from target: 0x79
16:30:09:903 : Sending number of bytes to be read - 1 and its checksum:
16:30:09:903 : #data sent successfully to target: 0x0ff0
16:30:09:904 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:09:904 : #ack Received response from target: 0x79
16:30:09:904 : Received 16 data bytes from target
16:30:09:904 : Sending GetID command and its XOR:
16:30:09:904 : #byte 0x02 sent successfully to target
16:30:09:904 : bytesToWrite before send = 1
16:30:09:904 : bFlushRet = 1, bytesToWrite after flush() = 1
16:30:09:904 : waitForBytesWritten Error : The wait operation timed out.
16:30:09:905 : #byte 0xFD sent successfully to target
16:30:09:905 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:09:905 : #ack Received response from target: 0x79
16:30:09:905 : Received 5 data bytes from target : 0x030001061f
16:30:09:905 : Sending GetID command and its XOR:
16:30:09:906 : #byte 0x02 sent successfully to target
16:30:09:906 : #byte 0xFD sent successfully to target
16:30:09:906 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:09:906 : #ack Received response from target: 0x79
16:30:09:907 : Received 5 data bytes from target : 0x030001061f
16:30:09:907 : UPLOADING ...
16:30:09:907 : Size : 1024 Bytes
16:30:09:907 : Address : 0x10040000
16:30:09:907 : Read progress:
16:30:09:908 : Sending Read command and its XOR:
16:30:09:908 : #byte 0x11 sent successfully to target
16:30:09:908 : bytesToWrite before send = 1
16:30:09:909 : bFlushRet = 1, bytesToWrite after flush() = 1
16:30:10:853 : waitForBytesWritten Error : The wait operation timed out.
16:30:10:874 : #byte 0xEE sent successfully to target
16:30:10:874 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:10:874 : #ack Received response from target: 0x79
16:30:10:881 : Sending Read address and its checksum:
16:30:10:881 : #data sent successfully to target: 0x1004000014
16:30:10:884 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:10:884 : #ack Received response from target: 0x79
16:30:10:885 : Sending number of bytes to be read - 1 and its checksum:
16:30:10:885 : #data sent successfully to target: 0xff00
16:30:10:885 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:10:885 : #ack Received response from target: 0x79
16:30:10:906 : Received 256 data bytes from target
16:30:10:906 : Sending Read command and its XOR:
16:30:10:906 : #byte 0x11 sent successfully to target
16:30:10:906 : #byte 0xEE sent successfully to target
16:30:10:906 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:10:907 : #ack Received response from target: 0x79
16:30:10:907 : Sending Read address and its checksum:
16:30:10:907 : #data sent successfully to target: 0x1004010015
16:30:10:907 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:10:907 : #ack Received response from target: 0x79
16:30:10:907 : Sending number of bytes to be read - 1 and its checksum:
16:30:10:907 : #data sent successfully to target: 0xff00
16:30:10:909 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:10:910 : #ack Received response from target: 0x79
16:30:10:940 : Received 256 data bytes from target
16:30:10:940 : Sending Read command and its XOR:
16:30:10:941 : #byte 0x11 sent successfully to target
16:30:10:941 : #byte 0xEE sent successfully to target
16:30:10:941 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:10:941 : #ack Received response from target: 0x79
16:30:10:941 : Sending Read address and its checksum:
16:30:10:941 : #data sent successfully to target: 0x1004020016
16:30:10:941 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:10:941 : #ack Received response from target: 0x79
16:30:10:941 : Sending number of bytes to be read - 1 and its checksum:
16:30:10:942 : #data sent successfully to target: 0xff00
16:30:10:942 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:10:942 : #ack Received response from target: 0x79
16:30:10:986 : Received 256 data bytes from target
16:30:10:987 : Sending Read command and its XOR:
16:30:10:987 : #byte 0x11 sent successfully to target
16:30:10:987 : #byte 0xEE sent successfully to target
16:30:10:987 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:10:987 : #ack Received response from target: 0x79
16:30:10:987 : Sending Read address and its checksum:
16:30:10:987 : #data sent successfully to target: 0x1004030017
16:30:10:987 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:10:987 : #ack Received response from target: 0x79
16:30:10:987 : Sending number of bytes to be read - 1 and its checksum:
16:30:10:987 : #data sent successfully to target: 0xff00
16:30:10:987 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:10:988 : #ack Received response from target: 0x79
16:30:10:988 : Received 256 data bytes from target
16:30:10:988 : Data read successfully
16:30:10:988 : Time elapsed during the read operation is: 00:00:01.136
16:30:12:007 : Sending GetID command and its XOR:
16:30:12:008 : #byte 0x02 sent successfully to target
16:30:12:008 : bytesToWrite before send = 1
16:30:12:008 : bFlushRet = 1, bytesToWrite after flush() = 1
16:30:12:095 : waitForBytesWritten Error : The wait operation timed out.
16:30:12:095 : #byte 0xFD sent successfully to target
16:30:12:096 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:12:096 : #ack Received response from target: 0x79
16:30:12:096 : Received 5 data bytes from target : 0x030001061f
16:30:12:096 : Sending GetID command and its XOR:
16:30:12:096 : #byte 0x02 sent successfully to target
16:30:12:096 : #byte 0xFD sent successfully to target
16:30:12:096 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:12:096 : #ack Received response from target: 0x79
16:30:12:097 : Received 5 data bytes from target : 0x030001061f
16:30:13:008 : Sending GetID command and its XOR:
16:30:13:008 : #byte 0x02 sent successfully to target
16:30:13:014 : #byte 0xFD sent successfully to target
16:30:13:014 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:13:014 : #ack Received response from target: 0x79
16:30:13:014 : Received 5 data bytes from target : 0x030001061f
16:30:13:015 : Sending GetID command and its XOR:
16:30:13:015 : #byte 0x02 sent successfully to target
16:30:13:015 : #byte 0xFD sent successfully to target
16:30:13:015 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:13:016 : #ack Received response from target: 0x79
16:30:13:016 : Received 5 data bytes from target : 0x030001061f
16:30:14:014 : Sending GetID command and its XOR:
16:30:14:015 : #byte 0x02 sent successfully to target
16:30:14:021 : #byte 0xFD sent successfully to target
16:30:14:021 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:14:022 : #ack Received response from target: 0x79
16:30:14:024 : Received 5 data bytes from target : 0x030001061f
16:30:14:024 : Sending GetID command and its XOR:
16:30:14:024 : #byte 0x02 sent successfully to target
16:30:14:024 : #byte 0xFD sent successfully to target
16:30:14:024 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:14:025 : #ack Received response from target: 0x79
16:30:14:025 : Received 5 data bytes from target : 0x030001061f
16:30:15:020 : Sending GetID command and its XOR:
16:30:15:020 : #byte 0x02 sent successfully to target
16:30:15:025 : #byte 0xFD sent successfully to target
16:30:15:029 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:15:029 : #ack Received response from target: 0x79
16:30:15:030 : Received 5 data bytes from target : 0x030001061f
16:30:15:030 : Sending GetID command and its XOR:
16:30:15:030 : #byte 0x02 sent successfully to target
16:30:15:030 : #byte 0xFD sent successfully to target
16:30:15:030 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:15:030 : #ack Received response from target: 0x79
16:30:15:033 : Received 5 data bytes from target : 0x030001061f
16:30:16:026 : Sending GetID command and its XOR:
16:30:16:027 : #byte 0x02 sent successfully to target
16:30:16:036 : #byte 0xFD sent successfully to target
16:30:16:037 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:16:037 : #ack Received response from target: 0x79
16:30:16:039 : Received 5 data bytes from target : 0x030001061f
16:30:16:040 : Sending GetID command and its XOR:
16:30:16:040 : #byte 0x02 sent successfully to target
16:30:16:040 : #byte 0xFD sent successfully to target
16:30:16:040 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:16:040 : #ack Received response from target: 0x79
16:30:16:041 : Received 5 data bytes from target : 0x030001061f
16:30:17:033 : Sending GetID command and its XOR:
16:30:17:033 : #byte 0x02 sent successfully to target
16:30:17:036 : #byte 0xFD sent successfully to target
16:30:17:038 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:17:038 : #ack Received response from target: 0x79
16:30:17:040 : Received 5 data bytes from target : 0x030001061f
16:30:17:040 : Sending GetID command and its XOR:
16:30:17:040 : #byte 0x02 sent successfully to target
16:30:17:041 : #byte 0xFD sent successfully to target
16:30:17:044 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:17:044 : #ack Received response from target: 0x79
16:30:17:050 : Received 5 data bytes from target : 0x030001061f
16:30:18:039 : Sending GetID command and its XOR:
16:30:18:040 : #byte 0x02 sent successfully to target
16:30:18:043 : #byte 0xFD sent successfully to target
16:30:18:046 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:18:047 : #ack Received response from target: 0x79
16:30:18:047 : Received 5 data bytes from target : 0x030001061f
16:30:18:047 : Sending GetID command and its XOR:
16:30:18:047 : #byte 0x02 sent successfully to target
16:30:18:047 : #byte 0xFD sent successfully to target
16:30:18:048 : #ack Received response from target: 0x79
16:30:18:051 : Received 5 data bytes from target : 0x7903000106
16:30:19:045 : Sending GetID command and its XOR:
16:30:19:045 : #byte 0x02 sent successfully to target
16:30:19:051 : #byte 0xFD sent successfully to target
16:30:19:054 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:19:054 : #ack Received response from target: 0x79
16:30:19:054 : Received 5 data bytes from target : 0x030001061f
16:30:19:054 : Sending GetID command and its XOR:
16:30:19:054 : #byte 0x02 sent successfully to target
16:30:19:055 : #byte 0xFD sent successfully to target
16:30:19:055 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:19:055 : #ack Received response from target: 0x79
16:30:19:056 : Received 5 data bytes from target : 0x030001061f
16:30:20:051 : Sending GetID command and its XOR:
16:30:20:052 : #byte 0x02 sent successfully to target
16:30:20:058 : #byte 0xFD sent successfully to target
16:30:20:062 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:20:062 : #ack Received response from target: 0x79
16:30:20:062 : Received 5 data bytes from target : 0x030001061f
16:30:20:062 : Sending GetID command and its XOR:
16:30:20:062 : #byte 0x02 sent successfully to target
16:30:20:062 : #byte 0xFD sent successfully to target
16:30:20:062 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:20:063 : #ack Received response from target: 0x79
16:30:20:063 : Received 5 data bytes from target : 0x030001061f
16:30:21:059 : Sending GetID command and its XOR:
16:30:21:059 : #byte 0x02 sent successfully to target
16:30:21:062 : #byte 0xFD sent successfully to target
16:30:21:067 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:21:067 : #ack Received response from target: 0x79
16:30:21:067 : Received 5 data bytes from target : 0x030001061f
16:30:21:067 : Sending GetID command and its XOR:
16:30:21:067 : #byte 0x02 sent successfully to target
16:30:21:068 : #byte 0xFD sent successfully to target
16:30:21:070 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:21:070 : #ack Received response from target: 0x79
16:30:21:070 : Received 5 data bytes from target : 0x030001061f
16:30:22:065 : Sending GetID command and its XOR:
16:30:22:066 : #byte 0x02 sent successfully to target
16:30:22:071 : #byte 0xFD sent successfully to target
16:30:22:075 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:22:076 : #ack Received response from target: 0x79
16:30:22:076 : Received 5 data bytes from target : 0x030001061f
16:30:22:076 : Sending GetID command and its XOR:
16:30:22:076 : #byte 0x02 sent successfully to target
16:30:22:076 : #byte 0xFD sent successfully to target
16:30:22:077 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:22:077 : #ack Received response from target: 0x79
16:30:22:077 : Received 5 data bytes from target : 0x030001061f
16:30:23:073 : Sending GetID command and its XOR:
16:30:23:073 : #byte 0x02 sent successfully to target
16:30:23:073 : #byte 0xFD sent successfully to target
16:30:23:073 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:23:073 : #ack Received response from target: 0x79
16:30:23:089 : Received 5 data bytes from target : 0x030001061f
16:30:23:090 : Sending GetID command and its XOR:
16:30:23:090 : #byte 0x02 sent successfully to target
16:30:23:090 : #byte 0xFD sent successfully to target
16:30:23:090 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:23:090 : #ack Received response from target: 0x79
16:30:23:090 : Received 5 data bytes from target : 0x030001061f
16:30:24:079 : Sending GetID command and its XOR:
16:30:24:080 : #byte 0x02 sent successfully to target
16:30:24:080 : #byte 0xFD sent successfully to target
16:30:24:085 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:24:085 : #ack Received response from target: 0x79
16:30:24:091 : Received 5 data bytes from target : 0x030001061f
16:30:24:091 : Sending GetID command and its XOR:
16:30:24:092 : #byte 0x02 sent successfully to target
16:30:24:092 : #byte 0xFD sent successfully to target
16:30:24:092 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:24:092 : #ack Received response from target: 0x79
16:30:24:092 : Received 5 data bytes from target : 0x030001061f
16:30:24:671 : UART PORT CLOSE
16:30:24:684 : Disconnected from device.
I think the problem on your side is to use the even parity.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.