Skip to main content
bvn123
Associate II
Feb 5, 2019 9:11 AM UTC
Question

Gerber for STEVAL-FKI433V2: number of layers (two or three) & holes (through or blind)

Hello,

I use two Evaluation boards STEVAL-FKI433V2 and now there is a task to order simpler and more compact PCB.

The STEVAL-FKIxxx Gerber archive

https://www.st.com/resource/en/board_manufacturing_specification/steval-fki433v2_gerber.zip

includes the file STEVAL-FKI433V2.G1, which contains GROUND plain, as is described in STEVAL-FKI433V2.EXTREP.

As I know, 4-layer PCB is simpler to order than 3-layer PCB.

This PCB may be routed using only 2 layers.

Question1: Has Evaluation board STEVAL-FKI433V2 three layers?

Question2: Are the GROUND holes THROUGH or BLIND type (if the Plane GROUND layer is used)?

Question3: Is the use of 2-layer PCB for S2-LP on 433MHz (without GROUND PLANE layer) a wrong decision?

    This topic has been closed for replies.

    1 reply

    bvn123
    bvn123Author
    Associate II
    Feb 7, 2019 5:17 PM UTC

    The questions are solved. I cut some part of PCB and divided it for the layers. The PLANE layer is placed approximately 0.3mm under TOP layer.