Skip to main content
Associate
May 27, 2024 5:54 PM UTC
Solved

FW-WBA v1.3.1: The code generated with this version doesn’t work.

Hi, I upgraded CubeIDE from 1.14.1 to 1.15.1 and CubeMX from 6.10.0 to 6.11.1. After the upgrade I built my code, and everything worked fine but I changed some parameters in CubeMX and tried to regenerate the code. CubeMX asked for upgrade of FW_WBA from 1.3.0 to 1.3.1 and I did this upgrade also.

STM32 Board: STM32WBA52CG

With FW_WBA v1.3.1:

1. There is a linker error:

E:/DevTools/ST/STM32CubeIDE_1.15.1/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.12.3.rel1.win32_1.0.100.202403111256/tools/bin/../lib/gcc/arm-none-eabi/12.3.1/../../../../arm-none-eabi/bin/ld.exe: warning: E:/DevTools/ST/STM32CubeIDE_1.15.1/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.12.3.rel1.win32_1.0.100.202403111256/tools/bin/../lib/gcc/arm-none-eabi/12.3.1/thumb/v8-m.main+fp/hard/crtn.o: missing .note.GNU-stack section implies executable stack

E:/DevTools/ST/STM32CubeIDE_1.15.1/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.12.3.rel1.win32_1.0.100.202403111256/tools/bin/../lib/gcc/arm-none-eabi/12.3.1/../../../../arm-none-eabi/bin/ld.exe: NOTE: This behavior is deprecated and will be removed in a future version of the linker.

2. Linker option -z noexecstack fixes the error.

3. The generated code crashes with Hard Fault in AMM_BackgroundProcess

HardFault_Handler() at stm32wbaxx_it.c:103 0x8007f34       

<signal handler called>() at 0xffffffbc              

_tx_thread_system_suspend() at tx_thread_system_suspend.c:85 0x80129a2             

_tx_semaphore_get() at tx_semaphore_get.c:214 0x8012284             

_txe_semaphore_get() at txe_semaphore_get.c:144 0x80139a4        

AMM_BackgroundProcess_Entry() at app_entry.c:549 0x8006cd2     

_tx_thread_shell_entry() at tx_thread_shell_entry.c:114 0x80126ac

<signal handler called>() at 0xffffffff

4. I've created a new project from scratch, and it has the same linker error and crashes the same way.

Tried with TreadX, FreeRTOS and Sequencer - no difference.

For me this version is unusable, and I have to go back to the previous ones.

This topic has been closed for replies.
STTwo-32
STTwo-32Best answer
ST Technical Moderator
Jun 27, 2024 3:41 PM UTC

Hello @KrassiNB 

This issue has been tracked for fix by this internal ticket:177107. It should be solved on the Coming release (very soon)

(PS: Internal ticket:177107 is an internal tracking number and is not accessible or usable outside of ST).

Thanks again for your contribution and do not hesitate to raise any issue/ feedback.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

3 replies

KrassiNBAuthor
Associate
May 27, 2024 8:26 PM UTC

Update:

I downgraded to the previous versions and there is no problem.

These are the versions that work:

STM32CubeMX 6.10.0

STM32CubeIDE 1.14.1

FW_WBA v1.2.0

 

STTwo-32
STTwo-32Best answer
ST Technical Moderator
Jun 27, 2024 3:41 PM UTC

Hello @KrassiNB 

This issue has been tracked for fix by this internal ticket:177107. It should be solved on the Coming release (very soon)

(PS: Internal ticket:177107 is an internal tracking number and is not accessible or usable outside of ST).

Thanks again for your contribution and do not hesitate to raise any issue/ feedback.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
ST Technical Moderator
Dec 12, 2024 1:17 PM UTC

Hi @KrassiNB ,

This issue is fixed with STM32CubeIDE 1.16.0: STM32CubeIDE:STM32CubeIDE errata 1.16.x - stm32mcu

Please update and use the latest release STM32CubeIDE 1.17.0.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks