Skip to main content
fo_it
Associate II
Aug 14, 2025 2:08 PM UTC
Question

FUS_STATE_IMG_NOT_AUTHENTIC during upgrading the FUS

Hello,

We try to upgrade the BLE stack to the latest 1.23.0. This version requires FUS v.2. We are unable to do this due to the FUS_STATE_IMG_NOT_AUTHENTIC error. We're using STM32CubeProgrammer v. 2.12.0. We have also tried with STM32CubeProgrammer v. 2.20.0following the steps in the release note of the binary files with the same result. 

Currently:

- FUS version: 1.2.0.0

- BLE stack version: 1.8.0.3.

 

We tried on both out custom board and on NUCLEO-WB44 with the same result. Could someone guide us to a solution?

Thanks in advance.

 

This topic has been closed for replies.

7 replies

STTwo-32
ST Technical Moderator
Aug 14, 2025 2:42 PM UTC

Hello @fo_it 

Could you please try to do that using the STM32CubeProgrammer V2.20.0.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
fo_it
fo_itAuthor
Associate II
Aug 14, 2025 3:40 PM UTC

Hello @STTwo-32 

I've tried  following on NUCLEO-WB55 using STM32CubeProgrammer v. 2.20.0:

- Upgrade to FUS v1.2.0 for verifying the process: Success

- Upgrade to FUS v2.0.0: Success

- Upgrade to FUS v2.1.0: Success

On our custom board none of the above was succeeded. We only get FUS_STATE_IMG_NOT_AUTHENTIC error.

STTwo-32
ST Technical Moderator
Aug 14, 2025 4:13 PM UTC

Could you please send the values of your option bytes, the current version of your FUS/STACK (on a screenshot from the STM32CubeProgrammer if possible) , the exact reference of your MCU and the files that you are using exactly. 

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
fo_it
fo_itAuthor
Associate II
Aug 15, 2025 6:23 AM UTC

The option bytes are:

STM32WB55RGV6 - Option Bytes.png

and the FUS information is:

STM32WB55RGV6 - FUS Information.png

We use both the FUS firmware and the stack firmware from stock firmware downloaded by the STM32CubeIDE. The MCU is STM32WB55RGV6.

fo_0-1755238981767.png

 

STTwo-32
ST Technical Moderator
Aug 15, 2025 8:47 AM UTC

Hello @fo_it 

Are you sure you are trying to flash the FUS to the correct address. If so, could you please perform a Mass erase before uploading any FUS file.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
fo_it
fo_itAuthor
Associate II
Aug 15, 2025 9:25 AM UTC

I do it  in exactly same way as I do with NUCLEO-WB55. I load the FUS v2.0.0.3 in the STM32CubeProgrammer v. 2.20.0 with the "Start address automatic determination" active. With the stack v1.22.0.2 already installed, the programming of FUS returns FUS_STATE_IMG_NO_SPACE. When the stack is deleted, then programming of FUS returns FUS_STATE_IMG_NOT_AUTHENTIC.

I've also tried with the start address 0x080EE000 manually with the same result.

STTwo-32
ST Technical Moderator
Sep 15, 2025 3:06 PM UTC

Hello @fo_it 

Could you please try to:

  • Set the RDP from level 0 to level 1 and set it back to level 0. After that update your FUS and Stack.
  • Upload a simple code to the board (GPIO_Toggle comme exemple) and try to update the FUS and stack after that.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.