FSK bandwidth selection documentation error?
In 5.5.3 FSK modem
BR = 32 x HSE32_freq / BitRate where HSE32_freq = 32 MHz
Fdev = Fdev[Hz] / FreqStep where FreqStep = HSE32_freq / 2^25
The document then states that to ensure correct modulation the following limit applies:
(Fdev + BR/2) < BW
In the Semtech document the limit is given as:
(2*Fdev + BR) < BW
What is the correct limit?
Does BW above actually refer to the values in the BW[DSB] column of Table 28 (also Semtech SX126x DS Table 6-4)?
The bandwidth must be chose so that:
BW[DSB] >= BR + 2 x frequency deviation + frequency error
Should the BR here be BitRate , and not the BR parameter which is referenced to the HSE32 frequency?