Question
Fixed Pin Pairing and Bonding with an STM32WB55
I am running the same firmware build on two different pieces of hardware that contain an STM32WB55CG. The firmware is configured to use a Fixed Pin for pairing and bonding. One works as expected and will create a bonded, authenticated, encrypted link but the other will not pair and bond. The one that works can be disconnected and power cycled. It works every time. I am not able to get the other one to work no matter what I try. There seems to be something simple that I am missing. Why would it work on one but not the other?