Skip to main content
islavv
Associate III
Aug 28, 2025 12:17 AM UTC
Question

Feedback on STM32WB55 Series Flash Architecture

My Feedback on STM32WB Series Flash Architecture

Dear STMicroelectronics Team,

As an experienced developer working  with the STM32WB series, I must voice a critical concern about its current flash memory architecture.

By placing both the Cortex‑M4 application and the Cortex‑M0+ wireless stack into a single shared internal flash, divided only by secure boundaries, you have created avoidable complexity and limitations for developers and end‑users alike. This design forces us to contend with:

  • Hard‑coded secure boundaries (SFSA/SBRV) and OB flags (DDS, C2OPT) that can only be altered via FUS or System Memory, making recovery unnecessarily difficult.

  • Loss of usable program space for the M4 when the wireless stack is present, even if the reserved region is unused.

  • Risk of total application downtime when the secure portion becomes corrupted or blocked, as both cores depend on the same physical array.

  • Debug and update processes that are far more fragile than they should be, especially in production environments.

For a platform intended to be versatile and developer‑friendly, these constraints create needless technical and operational overhead.

I strongly urge STMicroelectronics to consider, in future revisions of the STM32WB family, a dual‑flash architecture:

  • One physically independent flash array for the M4 application.

  • One dedicated, protected array for the M0+ wireless stack and secure services.

This separation would:

  • Eliminate cross‑core interference in flash access.

  • Simplify option byte logic and recovery scenarios.

  • Allow developers to fully utilize available program memory without jeopardizing wireless functionality.

  • Greatly improve the robustness and maintainability of deployed products.

This topic has been closed for replies.

1 reply

STTwo-32
ST Technical Moderator
Aug 28, 2025 12:32 PM UTC

Hello @islavv 

Thank you so much for this recommendation. I've escalated your remarks internally to be reviewed by our architecture team. 

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.