Skip to main content
W.K. Tam
Associate II
Aug 7, 2023 6:19 AM UTC
Question

Failed to read time and date in STMWLE5 software

I want to record the time of sensor activity in a program running in STM32WL MCU but only get the value of 0. The program is modified from the example LoRaWAN_End_Node. Below please find the RTC setting and the code to get the date and time. Can any expert help to solve the problem ?

< Codes in rtc.c>

/* RTC init function */
void MX_RTC_Init(void)
{

/* USER CODE BEGIN RTC_Init 0 */

/* USER CODE END RTC_Init 0 */

RTC_AlarmTypeDef sAlarm = {0};
RTC_TimeTypeDef sTime = {0}; // Added
RTC_DateTypeDef sDate = {0}; // Added
/* USER CODE BEGIN RTC_Init 1 */

/* USER CODE END RTC_Init 1 */

/** Initialize RTC Only
*/
hrtc.Instance = RTC;
hrtc.Init.HourFormat = RTC_HOURFORMAT_24; // Added
hrtc.Init.AsynchPrediv = RTC_PREDIV_A;
hrtc.Init.OutPut = RTC_OUTPUT_DISABLE;
hrtc.Init.OutPutRemap = RTC_OUTPUT_REMAP_NONE;
hrtc.Init.OutPutPolarity = RTC_OUTPUT_POLARITY_HIGH;
hrtc.Init.OutPutType = RTC_OUTPUT_TYPE_OPENDRAIN;
hrtc.Init.OutPutPullUp = RTC_OUTPUT_PULLUP_NONE;
// hrtc.Init.BinMode = RTC_BINARY_ONLY;
hrtc.Init.BinMode = RTC_BINARY_MIX; // added to try
hrtc.Init.BinMixBcdU = RTC_BINARY_MIX_BCDU_0; // added to try
if (HAL_RTC_Init(&hrtc) != HAL_OK)
{
Error_Handler();
}

/* USER CODE BEGIN Check_RTC_BKUP */

/* USER CODE END Check_RTC_BKUP */

/** Initialize RTC and set the Time and Date
*/
if (HAL_RTCEx_SetSSRU_IT(&hrtc) != HAL_OK)
{
Error_Handler();
}

/** Enable the Alarm A
*/
sAlarm.BinaryAutoClr = RTC_ALARMSUBSECONDBIN_AUTOCLR_NO;
sAlarm.AlarmTime.SubSeconds = 0x0;
sAlarm.AlarmMask = RTC_ALARMMASK_NONE;
sAlarm.AlarmSubSecondMask = RTC_ALARMSUBSECONDBINMASK_NONE;
sAlarm.Alarm = RTC_ALARM_A;
if (HAL_RTC_SetAlarm_IT(&hrtc, &sAlarm, 0) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN RTC_Init 2 */
sTime.Hours = 0x22;
sTime.Minutes = 0x30;
sTime.Seconds = 0x0;
sTime.DayLightSaving = RTC_DAYLIGHTSAVING_NONE;
sTime.StoreOperation = RTC_STOREOPERATION_RESET;
if (HAL_RTC_SetTime(&hrtc, &sTime, RTC_FORMAT_BCD) != HAL_OK)
{
Error_Handler();
}
sDate.WeekDay = RTC_WEEKDAY_MONDAY;
sDate.Month = RTC_MONTH_AUGUST;
sDate.Date = 0x07;
sDate.Year = 0x23;

if (HAL_RTC_SetDate(&hrtc, &sDate, RTC_FORMAT_BCD) != HAL_OK)
{
Error_Handler();
}
/* USER CODE END RTC_Init 2 */

}

<Codes in main.c>

// .... <other codes>.....

while (1)
{

//......<other codes>....

if (HAL_GPIO_ReadPin(GPIOC, GPIO_PIN_13) == GPIO_PIN_RESET) // Set to SET for product
{
HAL_RTC_GetTime(&hrtc, &sTime, RTC_FORMAT_BIN);
HAL_RTC_GetDate(&hrtc, &sDate, RTC_FORMAT_BIN);
sTamper.minutes = sTime.Minutes;
sTamper.hours = sTime.Hours;
sTamper.date = sDate.Date;
sTamper.month = sDate.Month;
sTamper.year = sDate.Year;
if (Tamper != 1)
{
// Call tamper event record routine to store tamper start time in EEPROM
// tamper_sRec();
}
// Call tamper event routine to upload tamper event payload
Tamper_event();
HAL_GPIO_WritePin(LED1_GPIO_Port, LED1_Pin, GPIO_PIN_SET); // for testing
sprintf((char*)tamtime, "Time: %02d.%02d\n\r", sTamper.hours, sTamper.minutes); // for testing
HAL_UART_Transmit(&huart2, tamtime, sizeof(tamtime), 300); // for testing
Tamper = 1;
tamper_eRec_flag = 0;
} else {
if (Tamper == 1)
{
HAL_RTC_GetTime(&hrtc, &sTime, RTC_FORMAT_BIN);
HAL_RTC_GetDate(&hrtc, &sDate, RTC_FORMAT_BIN);
eTamper.minutes = sTime.Minutes;
eTamper.hours = sTime.Hours;
eTamper.date = sDate.Date;
eTamper.month = sDate.Month;
eTamper.year = sDate.Year;
if (tamper_eRec_flag == 0)
{
// Call tamper event record routine to store tamper end time in EEPROM
// tamper_eRec();
tamper_eRec_flag = 1;
// Call tamper clear event routine to upload tamper clear payload
Tamper_clear();
}

HAL_GPIO_WritePin(LED1_GPIO_Port, LED1_Pin, GPIO_PIN_RESET); // for testing
} else {
Tamper = 0;
}
}
// Start ADC Conversion
HAL_ADC_Start(&hadc);
// Read the ADC value of PA11
if (HAL_ADC_PollForConversion(&hadc, 100)== HAL_OK)
{
adc_value = HAL_ADC_GetValue(&hadc);
}
// Convert the ADC value to voltage (millivolts)
millivolts = (adc_value * 3300) / 4096;

// Check if voltage is below alert threshold
if (millivolts < 2500) {
if (millivolts < 2000)
{
HAL_RTC_GetTime(&hrtc, &sTime, RTC_FORMAT_BIN);
HAL_RTC_GetDate(&hrtc, &sDate, RTC_FORMAT_BIN);
Bateol.minutes = sTime.Minutes;
Bateol.hours = sTime.Hours;
Bateol.date = sDate.Date;
Bateol.month = sDate.Month;
Bateol.year = sDate.Year;
if (BatteryEOL != 1)
{
// Store Battery EOL time in EEPROM
// BatteryEOL_Rec();
// Upload battery end of line time to server
battery_eol_time();
}

BatteryEOL = 1; // Set battery end of life flag
HAL_GPIO_TogglePin(GPIOB, LED1_Pin); // for testing
} else {
HAL_RTC_GetTime(&hrtc, &sTime, RTC_FORMAT_BIN);
HAL_RTC_GetDate(&hrtc, &sDate, RTC_FORMAT_BIN);
Batlow.minutes = sTime.Minutes;
Batlow.hours = sTime.Hours;
Batlow.date = sDate.Date;
Batlow.month = sDate.Month;
Batlow.year = sDate.Year;
if (Batterylow != 1)
{
// Store Battery low time in EEPROM
// BatteryLOW_Rec():
// Upload battery low time to server
battery_low_time();
}

Batterylow = 1; // Set battery low alert flag
BatteryEOL = 0; // reset battery end of life flag
HAL_GPIO_WritePin(GPIOB, LED1_Pin, GPIO_PIN_SET); // for testing
}
} else {
// Clear alert indicator
Batterylow = 0;
BatteryEOL = 0;
HAL_GPIO_WritePin(GPIOB, LED1_Pin, GPIO_PIN_RESET);
}
HAL_Delay(30);
}
/* USER CODE END 3 */
}

This topic has been closed for replies.

2 replies

ST Technical Moderator
Aug 7, 2023 3:25 PM UTC

Hello @W.K. Tam ,

Try adding below line before calling "MX_RTC_Init()":

hrtc.IsEnabled.RtcFeatures = UINT32_MAX; 

 

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
W.K. Tam
W.K. TamAuthor
Associate II
Aug 8, 2023 6:10 AM UTC

Hi Imen,

Thanks for your help. I found that the sample program LoRaWAN_End_Node does not call "MX_RTC_Init()". How does it configure and use the RTC ? I tried to add the "MX_RTC_Init()" in the user code section with your suggested line below put before. I still got the zero in the time - hour and minute.

hrtc.IsEnabled.RtcFeatures = UINT32_MAX; 

Regards,

W.K. Tam