Fail und FUS and Stack update
- 9 replies
- 2542 views
Hi everybody,
I think I have the same problem as CTare (https://community.st.com/s/question/0D53W00000fo0kcSAA/unable-to-install-wireless-stack-on-stm32wb55?t=1628516513992) I coudn't reply to that post because it's already archived.
My setup: Nucleo WB55RG board. I tried to fully understand the FUS, Stack programming including all the options. After 6hours I end up with a board that I can communicate with using STM32Programmer (v2.8, 2.7 and 2.5, each of them in DFU or STlink mode) but I'm not able to reprogram FUS and RF-Stack (in my case BLE). I attached my batch file that is derived from Quintin and the response the board gives (because of the limitations in this forum as one pdf file :worried_face:). What makes me very suspicious is the FUS firmware version that is replied to be v0.0.0.00 (that's the same I can see in STM32Programmer. So it seems to me that there is no FUS at all - although the programming command don't show errors.
Similar to CTare I'm not sure if I hit the 'antirollback' push button accidentially. Following the previous post I tried to fix that with STM32Programmer v2.5 but with no sucess. Is there really no way to remove that antirollback flag somewhere in the STM32WB?
Anybody any idea what went wrong and how to fix this?
Best Regards
Markus