Skip to main content
DavePfz
Senior
Feb 24, 2026 10:15 PM UTC
Solved

Expansion Board with Quad SPI NOR FLASH

Are there any expansion boards with Quad SPI NOR Flash chips? I am interested in using it with a NUCLEO-WB55RG board.Preferably it should use the Macronix 25L6433FM2I-08G chip, but that is not a hard requirement. This chip is found on the X-NUCLEO-GFX01M2 board, but it is implemented as a standard single SPI interface.

Thanks

Imen.DBest answer
ST Technical Moderator
Mar 9, 2026 1:05 PM UTC

Hello @DavePfz ,

I did not find an expansion board for the Nucleo-WB55RG that includes a Quad-SPI NOR flash memory. You can use a Discovery board, such as the STM32WB5MM-DK board, which supports Quad-SPI mode and embeds a 128-Mbit Quad-SPI NOR Flash Memory.
In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks

2 replies

Imen.DBest answer
ST Technical Moderator
Mar 9, 2026 1:05 PM UTC

Hello @DavePfz ,

I did not find an expansion board for the Nucleo-WB55RG that includes a Quad-SPI NOR flash memory. You can use a Discovery board, such as the STM32WB5MM-DK board, which supports Quad-SPI mode and embeds a 128-Mbit Quad-SPI NOR Flash Memory.
In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
DavePfz
DavePfzAuthor
Senior
Mar 9, 2026 1:10 PM UTC

Thanks for looking into this. I came to the same conclusion. Although the STM32WB5MM-DK was not exactly what I was looking for it did give me the information I needed.

Thanks