Skip to main content
ANist
Associate III
Sep 25, 2019 7:49 PM UTC
Solved

Error when updating FUS firmware

I am trying to update the FUS firmware to the latest version on a STM32WB55CG, following the guide in the release notes I get Error: Firmware not authentic!. at step 5 (RSS_IMAGE_NOT_AUTHENTIC).

I have the latest CubeProg version and my actual FUS is 0.5.3

Am I doing something wrong?

Thanks!

This topic has been closed for replies.
ANist
ANistBest answer
Associate III
Sep 27, 2019 12:49 PM UTC

@Remi QUINTIN​  SOLVED: as found in another post in this forum https://community.st.com/s/question/0D50X0000Ap44FlSQI/restore-stm32wb55-fus-firmware), I set the read protection byte to 0xBB and then back to 0xAA. After that I was able to upgrade to FUS 1.0.1, you may want to investigate this behavior or wrtite it on some documentation.

Thanks again for your help!

23 replies

ANist
ANistAuthor
Associate III
Sep 27, 2019 12:41 PM UTC

Sorry to hear that, here the list of option bytes taken from CLI:

OPTION BYTES BANK: 0
 
 Read Out Protection:
 
 RDP : 0xAA (Level 0, no protection)
 
 BOR Level:
 
 BOR_LEV : 0x0 (BOR Level 0 reset level threshold is around 1.7 V)
 
 User Configuration:
 
 nBOOT0 : 0x1 (nBOOT0=1)
 nBOOT1 : 0x1 (Boot from code area if BOOT0=0 otherwise embedded SRAM)
 nSWBOOT0 : 0x1 (BOOT0 taken from PH3/BOOT0 pin)
 SRAM2RST : 0x0 (SRAM2 erased when a system reset occurs)
 SRAM2PE : 0x1 (SRAM2 parity check disable)
 nRST_STOP : 0x1 (No reset generated when entering the Stop mode)
 nRST_STDBY : 0x1 (No reset generated when entering the Standby mode)
 nRSTSHDW : 0x1 (No reset generated when entering the Shutdown mode)
 WWDGSW : 0x1 (Software window watchdog)
 IWGDSTDBY : 0x1 (Independent watchdog counter running in Standby mode)
 IWDGSTOP : 0x1 (Independent watchdog counter running in Stop mode)
 IWDGSW : 0x1 (Software independent watchdog)
 IPCCDBA : 0x0 (0x0)
 
 Security Configuration Option bytes:
 
 ESE : 0x1 (Security enabled)
 SFSA : 0xF6 (0xF6)
 FSD : 0x0 (System and Flash secure)
 DDS : 0x1 (CPU2 debug access disabled)
 C2OPT : 0x1 (SBRV will address Flash)
 NBRSD : 0x0 (SRAM2b is secure)
 SNBRSA : 0x10 (0x10)
 BRSD : 0x1 (SRAM2a is non-secure)
 SBRSA : 0x0 (0x0)
 SBRV : 0x3D800 (0x3D800)
 
 PCROP Protection:
 
 PCROP1A_STRT : 0x1FF (0x8000FF8)
 PCROP1A_END : 0x0 (0x8000008)
 PCROP_RDP : 0x0 (PCROP zone is kept when RDP is decreased)
 PCROP1B_STRT : 0x1FF (0x8000FF8)
 PCROP1B_END : 0x0 (0x8000008)
 
 Write Protection:
 
 WRP1A_STRT : 0xFF (0x807F800)
 WRP1A_END : 0x0 (0x8000000)
 WRP1B_STRT : 0xFF (0x807F800)
 WRP1B_END : 0x0 (0x8000000)

What is curious is that I am able to flash ble stack from version 1.0.0, which event generates the "firmware not authentic" error?

ANist
ANistAuthorBest answer
Associate III
Sep 27, 2019 12:49 PM UTC

@Remi QUINTIN​  SOLVED: as found in another post in this forum https://community.st.com/s/question/0D50X0000Ap44FlSQI/restore-stm32wb55-fus-firmware), I set the read protection byte to 0xBB and then back to 0xAA. After that I was able to upgrade to FUS 1.0.1, you may want to investigate this behavior or wrtite it on some documentation.

Thanks again for your help!

abbas14
Associate III
Mar 13, 2020 11:17 AM UTC

Thank you, @Andrea Nisticò​, for suggesting that solution.

Tried that, and my controller is now permanently read-protected! I am unable to revert it to its normal functionality.

Please find attached screenshots of the current status of the option bytes.

0693W000000TrtRQAS.png0693W000000TrtWQAS.png

0693W000000TrtbQAC.png0693W000000TrtvQAC.png

0693W000000Tru0QAC.png

It would be really appreciable if anyone could guide me to the current state of my device, and whether it is recoverable.

Remi QUINTIN
ST Technical Moderator
Sep 27, 2019 1:03 PM UTC

​Great!!!!

Indeed I will have a look at this strange influence of the RDP option byte on the ability to upgrade the FUS.

The fact that this action is erasing all data from the start of the flash up to the SFSA pointer may lead to the possibility of an incomplete erasure done by the CLI command "STM32_Programmer_CLI.exe -c port=usb1 -fwdelete".

I will check this.

thanks

Remi QUINTIN
ST Technical Moderator
Mar 9, 2020 10:32 AM UTC

​So let's resume this topic

Be sure to use the latest CuveWB FW package v1.5.0.

Then could you tell me which port you are using?

Remi QUINTIN
ST Technical Moderator
Mar 13, 2020 12:55 PM UTC

What is the CubeWB FW package version you are using?

What is the FUS version?

abbas14
Associate III
Mar 13, 2020 2:55 PM UTC

CubeWB FW package version: 1.5

FUS version: The original (0.5.3)

All update attempts are unsuccessful.

Remi QUINTIN
ST Technical Moderator
Mar 13, 2020 3:50 PM UTC

I Just saw that the SFSA pointer is set to 0. This is not a good news.

Did you never manage to upgrade the FUS on this Nucleo board?

Which port did you use?

Were you able to load FUS v1.1.0, I would be able to recover from this situation.

Now there is nothing obvious to do.

abbas14
Associate III
Mar 16, 2020 8:02 AM UTC

Nope, I was never able to upgrade this device!

I just set the read protection byte to 0xBB (from the default 0xAA), and it's stuck since then.

This device is on a custom board, and is being programmed through ST-Link.

Mar 18, 2020 3:25 PM UTC

I was getting such as error. But after typing STM32_Programmer_CLI.exe -c port=usb1 -r32 0x20030030 1 it showed that the firmware has been updated. I was seeing 0x20030030 00000000 but now I see 01000200. Anyway it doesn't work.

Remi QUINTIN
ST Technical Moderator
Mar 18, 2020 3:59 PM UTC

So the FUS had indeed been upgraded. Unfortunately, this is not enough to get your board back to work as the SFSA pointer = 0.

This is a quite weird situation as this sequence should not failed , leading to this blocked board.