Skip to main content
anddam
Associate
Jun 25, 2020 11:01 AM UTC
Question

Error upgrading wireless coprocessor firmware on Nucleo-68

I am experiencing an error while trying to upgrade a Nucleo-68 board from P-NUCLEO-WB55 wireless coprocessor to latest v1.7.0 firmware provided by STMicroelectronics/STM32CubeWB github repo.

I already reported the issue on the githb repo here is a copy of the issue:

**Describe the set-up**

Host OS: Linux glibc system

Board: P-NUCLEO-WB55 STM32WB55RG (Nucleo-68)

Tools:

 - STM32CubeProgrammer v2.4.0

 - SMT32CubeWB firmware images

**Describe the bug**

Trying to update the wireless coprocessor to latest v1.7.0 results in an error:

```

Error: failed to download Segment[0]

Error: failed to download the File

Error: Failed to download image!

```

**How To Reproduce**

1. clone `https://github.com/STMicroelectronics/STM32CubeWB`

2. enter the repository

3. checkout tag `v1.7.0`

4. cd `Projects/STM32WB_Copro_Wireless_Binaries/STM32WB5x/`

5. follow instructions at `How to flash the Wireless Coprocessor Binary via USB (Command Line Interface)` in file `Release_Notes.html` using STM32CubeProgrammer v2.4.0

**Additional context**

The *Update History* section of `Release_Notes.html` shows 1.6.0 changes as latest entry even on tag `v.1.7.0`. However checking out the repo at `v1.6.0` yields the same error result as `v1.7.0`.

The full log provided in the issue is attached here as well.

This topic has been closed for replies.

17 replies

Remi QUINTIN
ST Technical Moderator
Jul 3, 2020 9:39 AM UTC

​You can use CubeProgrammer tool in GUI mode and read the sector you want to erase. Try to write some data and activate the masse erase. Then check if the data you wrote is indeed erased.

Remi QUINTIN
ST Technical Moderator
Jul 3, 2020 10:23 AM UTC

​No.  as long as nSWBOOT0 = 0x1  and the jumper is properly set, I dont see any reason for such error.

What is the voltage used to power your board?

anddam
anddamAuthor
Associate
Aug 9, 2020 9:59 PM UTC

The voltage is the 5 V from host USB via the USB_user port, the source is set via "USB MCU" jumper.

Sorry for the delayed reply.