Skip to main content
Jun 4, 2020 3:31 AM UTC
Question

Error: --Reserved -- in CubeProgrammer 2.4

Hello! I am trying to download the FUS V1.1.0.0 to a STM32WB5xE controller through SWD in CubeProgrammer so as to update the firmware. But I receive Error: --Reserved-- . I ignored it and downloaded the firmware successfuly but my BLE stack doesn't work :( . I have soldered the controller in my board and connected some peripherals to him and everything is working ех�?еpt BLE. What can I do? Here is the log of CubeProgrammer:

06:13:42 : STM32CubeProgrammer API v2.4.0

06:14:37 : ST-LINK SN : 2A3009013212354D434B4E00

06:14:37 : ST-LINK FW : V2J36S7

06:14:37 : Voltage : 3.19V

06:14:37 : SWD freq : 4000 KHz

06:14:37 : Connect mode: Under Reset

06:14:37 : Reset mode : Software reset

06:14:37 : Device ID : 0x495

06:14:38 : UPLOADING OPTION BYTES DATA ...

06:14:38 : Bank : 0x00

06:14:38 : Address : 0x58004020

06:14:38 : Size : 104 Bytes

06:14:38 : UPLOADING ...

06:14:38 : Size : 1024 Bytes

06:14:38 : Address : 0x8000000

06:14:38 : Read progress:

06:14:38 : Data read successfully

06:14:38 : Time elapsed during the read operation is: 00:00:00.007

06:15:16 : Old Firmware delete ...

06:15:16 : Warning: Option Byte: nSWboot0, value: 0x0, was not modified.

06:15:16 : Warning: Option Byte: nboot0, value: 0x1, was not modified.

06:15:16 : Warning: Option Byte: nboot1, value: 0x1, was not modified.

06:15:16 : Warning: Option Bytes are unchanged, Data won't be downloaded

06:15:16 : Succeeded to set nSWboot0=0 nboot1=1 nboot0=1 

06:15:16 : Memory Programming ...

06:15:16 : Opening and parsing file: 0x495_FUS_Operator.bin

06:15:16 : File : 0x495_FUS_Operator.bin

06:15:16 : Size : 11584 Bytes

06:15:16 : Address : 0x08000000 

06:15:16 : Erasing memory corresponding to segment 0:

06:15:16 : Erasing internal memory sectors [0 2]

06:15:16 : Download in Progress:

06:15:17 : File download complete

06:15:17 : Time elapsed during download operation: 00:00:00.686

06:15:17 : Application is running

06:15:25 : Reconnecting...

06:15:25 : Reconnected !

06:15:26 : Firmware delete Success

06:15:26 : Download Stack/FUS image at address 0x807a000 ...

06:15:26 : Memory Programming ...

06:15:26 : Opening and parsing file: stm32wb5x_FUS_fw.bin

06:15:26 : File : stm32wb5x_FUS_fw.bin

06:15:26 : Size : 24492 Bytes

06:15:26 : Address : 0x0807A000 

06:15:26 : Erasing memory corresponding to segment 0:

06:15:26 : Erasing internal memory sectors [122 127]

06:15:26 : Download in Progress:

06:15:27 : File download complete

06:15:27 : Time elapsed during download operation: 00:00:01.052

06:15:27 : Firmware Upgrade process started ...

06:15:27 : Application is running

06:15:37 : Reconnecting...

06:15:37 : Reconnected !

06:15:37 : Error: -- Reserved --

06:15:37 : Old Firmware delete ...

06:15:37 : Warning: Option Byte: nSWboot0, value: 0x0, was not modified.

06:15:37 : Warning: Option Byte: nboot0, value: 0x1, was not modified.

06:15:37 : Warning: Option Byte: nboot1, value: 0x1, was not modified.

06:15:37 : Warning: Option Bytes are unchanged, Data won't be downloaded

06:15:37 : Succeeded to set nSWboot0=0 nboot1=1 nboot0=1 

06:15:37 : Memory Programming ...

06:15:37 : Opening and parsing file: 0x495_FUS_Operator.bin

06:15:37 : File : 0x495_FUS_Operator.bin

06:15:37 : Size : 11584 Bytes

06:15:37 : Address : 0x08000000 

06:15:37 : Erasing memory corresponding to segment 0:

06:15:38 : Erasing internal memory sectors [0 2]

06:15:38 : failed to erase memory

06:15:38 : failed to erase memory

06:15:38 : Failed to download FUS operator!

06:15:38 : Retry -- 0

06:15:38 : Old Firmware delete ...

06:15:38 : Warning: Option Byte: nSWboot0, value: 0x0, was not modified.

06:15:38 : Warning: Option Byte: nboot0, value: 0x1, was not modified.

06:15:38 : Warning: Option Byte: nboot1, value: 0x1, was not modified.

06:15:38 : Warning: Option Bytes are unchanged, Data won't be downloaded

06:15:38 : Succeeded to set nSWboot0=0 nboot1=1 nboot0=1 

06:15:38 : Memory Programming ...

06:15:38 : Opening and parsing file: 0x495_FUS_Operator.bin

06:15:38 : File : 0x495_FUS_Operator.bin

06:15:38 : Size : 11584 Bytes

06:15:38 : Address : 0x08000000 

06:15:38 : Erasing memory corresponding to segment 0:

06:15:38 : Erasing internal memory sectors [0 2]

06:15:38 : Download in Progress:

06:15:38 : File download complete

06:15:38 : Time elapsed during download operation: 00:00:00.694

06:15:38 : Application is running

06:15:46 : Reconnecting...

06:15:47 : Reconnected !

06:15:48 : Firmware delete Success

06:15:48 : Download Stack/FUS image at address 0x807a000 ...

06:15:48 : Memory Programming ...

06:15:48 : Opening and parsing file: stm32wb5x_FUS_fw.bin

06:15:48 : File : stm32wb5x_FUS_fw.bin

06:15:48 : Size : 24492 Bytes

06:15:48 : Address : 0x0807A000 

06:15:48 : Erasing memory corresponding to segment 0:

06:15:48 : Erasing internal memory sectors [122 127]

06:15:48 : Download in Progress:

06:15:49 : File download complete

06:15:49 : Time elapsed during download operation: 00:00:00.923

06:15:49 : Firmware Upgrade process started ...

06:15:49 : Application is running

06:15:59 : Reconnecting...

06:15:59 : Reconnected !

06:15:59 : Error: -- Reserved --

06:15:59 : Old Firmware delete ...

06:15:59 : Warning: Option Byte: nSWboot0, value: 0x0, was not modified.

06:15:59 : Warning: Option Byte: nboot0, value: 0x1, was not modified.

06:15:59 : Warning: Option Byte: nboot1, value: 0x1, was not modified.

06:15:59 : Warning: Option Bytes are unchanged, Data won't be downloaded

06:15:59 : Succeeded to set nSWboot0=0 nboot1=1 nboot0=1 

06:15:59 : Memory Programming ...

06:15:59 : Opening and parsing file: 0x495_FUS_Operator.bin

06:15:59 : File : 0x495_FUS_Operator.bin

06:15:59 : Size : 11584 Bytes

06:15:59 : Address : 0x08000000 

06:15:59 : Erasing memory corresponding to segment 0:

06:15:59 : Erasing internal memory sectors [0 2]

06:15:59 : failed to erase memory

06:15:59 : failed to erase memory

06:15:59 : Failed to download FUS operator!

06:15:59 : Retry -- 1

06:15:59 : Old Firmware delete ...

06:15:59 : Warning: Option Byte: nSWboot0, value: 0x0, was not modified.

06:15:59 : Warning: Option Byte: nboot0, value: 0x1, was not modified.

06:15:59 : Warning: Option Byte: nboot1, value: 0x1, was not modified.

06:15:59 : Warning: Option Bytes are unchanged, Data won't be downloaded

06:15:59 : Succeeded to set nSWboot0=0 nboot1=1 nboot0=1 

06:15:59 : Memory Programming ...

06:15:59 : Opening and parsing file: 0x495_FUS_Operator.bin

06:15:59 : File : 0x495_FUS_Operator.bin

06:15:59 : Size : 11584 Bytes

06:15:59 : Address : 0x08000000 

06:15:59 : Erasing memory corresponding to segment 0:

06:15:59 : Erasing internal memory sectors [0 2]

06:15:59 : Download in Progress:

06:16:00 : File download complete

06:16:00 : Time elapsed during download operation: 00:00:00.590

06:16:00 : Application is running

06:16:08 : Reconnecting...

06:16:08 : Reconnected !

06:16:09 : Firmware delete Success

06:16:09 : Download Stack/FUS image at address 0x807a000 ...

06:16:09 : Memory Programming ...

06:16:09 : Opening and parsing file: stm32wb5x_FUS_fw.bin

06:16:09 : File : stm32wb5x_FUS_fw.bin

06:16:09 : Size : 24492 Bytes

06:16:09 : Address : 0x0807A000 

06:16:09 : Erasing memory corresponding to segment 0:

06:16:09 : Erasing internal memory sectors [122 127]

06:16:09 : Download in Progress:

06:16:10 : File download complete

06:16:10 : Time elapsed during download operation: 00:00:00.964

06:16:10 : Firmware Upgrade process started ...

06:16:10 : Application is running

06:16:20 : Reconnecting...

06:16:20 : Reconnected !

06:16:20 : Error: -- Reserved --

06:16:20 : Old Firmware delete ...

06:16:20 : Warning: Option Byte: nSWboot0, value: 0x0, was not modified.

06:16:20 : Warning: Option Byte: nboot0, value: 0x1, was not modified.

06:16:20 : Warning: Option Byte: nboot1, value: 0x1, was not modified.

06:16:20 : Warning: Option Bytes are unchanged, Data won't be downloaded

06:16:20 : Succeeded to set nSWboot0=0 nboot1=1 nboot0=1 

06:16:20 : Memory Programming ...

06:16:20 : Opening and parsing file: 0x495_FUS_Operator.bin

06:16:20 : File : 0x495_FUS_Operator.bin

06:16:20 : Size : 11584 Bytes

06:16:20 : Address : 0x08000000 

06:16:20 : Erasing memory corresponding to segment 0:

06:16:20 : Erasing internal memory sectors [0 2]

06:16:20 : failed to erase memory

06:16:20 : failed to erase memory

06:16:20 : Failed to download FUS operator!

06:16:20 : Retry -- 2

This topic has been closed for replies.

25 replies

Remi QUINTIN
ST Technical Moderator
Jun 16, 2020 1:58 PM UTC

You should perform a mass erase of the user part of the memory => RDP set to 0xBB and then back to 0xAA before programming your application.

Jun 16, 2020 2:31 PM UTC

my data is between 0x08000000 and 0x08004D90

Jun 18, 2020 6:13 AM UTC

I could flash my app in 0x08000000. I only ignored the adress out of range error. My data is between 0x08000000 and 0x08004D90.

I performed a full erase but it didn't help :crying_face:

I have two boards . The same app in the other board works properly.

Remi QUINTIN
ST Technical Moderator
Jun 18, 2020 12:49 PM UTC

Just two things in last resort

1) Use hw reset as the default reset mode in the GUI of CubeProgrammer

2) There are many some digits hidden in the window dedicated to the load address that generate an “out of range�? value? I got some issue with that in the past.

Jun 19, 2020 1:05 AM UTC

here is my window0693W000001r2RnQAI.png

when i click on "ok" it downloads the binary. When I reconnect, in Device memory he appears in the wanted address 0x08000000

Remi QUINTIN
ST Technical Moderator
Jun 19, 2020 7:25 AM UTC

>>I have two boards . The same app in the other board works properly.

So it is a board issue. I will try to get more explaination on the "reserved" error.

I really dont udertsand why you get this "address out of range" error.

I hibk it is 2 different problems.

Jun 19, 2020 8:17 PM UTC

Ok.

could you get a look at my options bytes? to check if it is allright there

Remi QUINTIN
ST Technical Moderator
Jun 21, 2020 6:01 PM UTC

Yes. So could you download them here so that I can check them?

Jun 22, 2020 12:06 AM UTC

0693W000001r8yOQAQ.png0693W000001r8yJQAQ.png0693W000001r8yEQAQ.png0693W000001r8y9QAA.png

Remi QUINTIN
ST Technical Moderator
Jun 22, 2020 9:17 AM UTC

There is absolutely nothing wrong regarding the values of the option bytes.

So lets go back to basics:

Could you use the batch file I joint to this tread and use it in CLI mode?

Just adapt the paths to you own configuration. (path with ****************)

No need to update the FUS, lets focus on the RF FW.

In the end, there is may be a HW issue with your RF part on this specific custom board.