Skip to main content
MMitc
Associate III
Oct 3, 2019 12:24 AM UTC
Question

Dongle does not show up as COM Port using BLE_TransparentModeVCP_reference.hex

I have WB55 Dongle board that someone may have programmed previously. I am trying to start it fresh and make sure it is up to date using all files from  from STM32Cube_FW_WB_V1.2.0

I followed the procedure to install new FUS and BLE Stack:

  1. STM32_Programmer_CLI.exe" -c port=usb1 -fwdelete
  2. STM32_Programmer_CLI.exe"  -c port=usb1 -fwupgrade stm32wb5x_FUS_fw.bin 0x080EC000 firstinstall=0
  3. STM32_Programmer_CLI.exe"  -c port=usb1 -fwupgrade "stm32wb5x_BLE_Stack_fw.bin" 0x080CC000 firstinstall=1

Then I used the Programmer in USB mode to download BLE_TransparentModeVCP_reference.hex

All that seems to work fine.

But when I set the switch back to normal boot and plug it in, there are no lights, and no COM port is recognized. Ironically, before I did this, the device did show up on COM3, but it was also unresponsive.

What did I do wrong, or how can I figure what is wrong?

This topic has been closed for replies.

13 replies

MMitc
MMitcAuthor
Associate III
Oct 7, 2019 4:23 PM UTC

Do you have any other suggestions or should I give up on this Dongle?

Remi QUINTIN
ST Technical Moderator
Oct 7, 2019 7:17 PM UTC

​Unfortunately I have absolutely no clue about the possible cause of this strange behavior.

I will come back to you if someone give me a new idea.

Till this potential feedback, you should let this dongle aside.

MLiva
Associate III
Oct 9, 2019 8:32 PM UTC

I have converted the .hex file to a .dfu and then use the ST dfu loader app to program the dongle and it works. The usb dongle reports as virtual com. You can even try to rebuild the .hex file as the sources are also in the V1.2.0 CubeFW package.