Skip to main content
Scott Dev
Senior
Feb 14, 2022 12:03 PM UTC
Question

Does the STM32WLEx have the SX126 built in? I have a LoRa-E5 module, and wondered what the difference is. Many Thanks Scott

..

This topic has been closed for replies.

6 replies

Peter BENSCH
ST Technical Moderator
Feb 14, 2022 12:41 PM UTC

The STM32WLE contains a licensed IP from Semtech, but no SX126x. The reference manual RM0453 RM0461 (see below) lists all the features of the contained LoRa® part.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Tesla DeLorean
Guru
Feb 14, 2022 1:01 PM UTC

The implementation is done on a single die, rather than a stacked die using a discreet SX126x.

The connection is via an internally routed SPI.

The register set/programming for LoRa should be materially the same as for an SX1262​

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Strooom
Senior
Mar 21, 2023 8:06 AM UTC

Hello @Peter BENSCH​  I think the reference manual for the STM32WLE is RM0461.

The RM0453 you mention is for the SMT32WL family.

Peter BENSCH
ST Technical Moderator
Mar 21, 2023 8:11 AM UTC

Thank you for pointing that out, I had actually mixed it up by mistake. Yes, RM0461 is the correct reference manual for the STM32WLE.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Strooom
Senior
Mar 21, 2023 8:29 AM UTC

You are welcome. If you have experience with the STM32WLE, please take a look at my problem STM32WLE5 'Failure To Execute Command' - I read the reference manual and search the forum, but I can't find an answer to this..