Skip to main content
JAnth
Visitor II
Aug 26, 2019 7:35 PM UTC
Question

Does the B-L072Z-LRWAN1 support I2C in both slave/master mode.

I wish to connect this kit (STM32L072CZY6TR) to a raspberry pi. As the Pi only supports SPI in master mode I need to use I2C to get a two way conversation.

I wish to send and receive the occasional codes from a server via LORAWAN and communicate those to a Raspberry Pi which in turn will control machinary. It is impossible for the Pi to be connected to the internet. I am hoping to not have to go down the GSM route.

Many thanks

This topic has been closed for replies.

1 reply

Tesla DeLorean
Guru
Aug 26, 2019 9:15 PM UTC

It will do whatever you program into it. You'll have to write the I2C support code.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..