Skip to main content
Batuhan A.
Associate III
Jun 10, 2021 8:24 AM UTC
Solved

Do I have to use a 32 kHz oscillator (LSE) for the STM32WB55 MCU ZigBee application?

Hello,

I am going to use a 32 MHz oscillator (LSE) for a ZigBee application on STM32WB55. Do I have to add a 32 kHz oscillator? I do not need RTC.

Best regards,

Batuhan

This topic has been closed for replies.
Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
Jun 14, 2021 4:50 PM UTC

You can use the STM32WB55 without the LSE if you:

  • don't need an RTC and
  • don't need beaconing support and
  • don't want to synchronize internal oscillators from LSE

If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.

Good luck!

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

1 reply

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
Jun 14, 2021 4:50 PM UTC

You can use the STM32WB55 without the LSE if you:

  • don't need an RTC and
  • don't need beaconing support and
  • don't want to synchronize internal oscillators from LSE

If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.

Good luck!

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.