Skip to main content
JakBSIP
Associate II
Sep 9, 2021 9:19 AM UTC
Question

Direct Connection Issue after Scanning

Hi there,

In short I am trying to use the Nucleo-68 board to scan for Cadence Sensor devices with UUID 0x1816 which I've managed successfully. I get a list of all available devices and their addresses (double checked against a report generated through my phone). However the issue arises when I issue a connect request - I do get a BLE_STATUS_SUCCESS (Green LED on) but the event callback hci_le_connection_complete_event() is never actually called because the Blue LED never turns on.

// Snippet of Connect_Request()

if (result == BLE_STATUS_SUCCESS) {

/* USER CODE BEGIN BLE_CONNECT_SUCCESS */

HAL_GPIO_WritePin(LED_GREEN_GPIO_Port, LED_GREEN_Pin, GPIO_PIN_SET);

/* USER CODE END BLE_CONNECT_SUCCESS */

BleApplicationContext.Device_Connection_Status =

APP_BLE_LP_CONNECTING;

} else {

/* USER CODE BEGIN BLE_CONNECT_FAILED */

HAL_GPIO_WritePin(LED_RED_GPIO_Port, LED_RED_Pin, GPIO_PIN_SET);

/* USER CODE END BLE_CONNECT_FAILED */

BleApplicationContext.Device_Connection_Status = APP_BLE_IDLE;

}

//Snippet of SVCCTL_App_Notification()

case HCI_LE_META_EVT_CODE: {

/* USER CODE BEGIN EVT_LE_META_EVENT */

/* USER CODE END EVT_LE_META_EVENT */

meta_evt = (evt_le_meta_event*) event_pckt->data;

switch (meta_evt->subevent) {

/* USER CODE BEGIN subevent */

/* USER CODE END subevent */

case HCI_LE_CONNECTION_COMPLETE_SUBEVT_CODE:

/* USER CODE BEGIN EVT_LE_CONN_COMPLETE */

HAL_GPIO_WritePin(LED_BLUE_GPIO_Port, LED_BLUE_Pin, GPIO_PIN_SET);

/* USER CODE END EVT_LE_CONN_COMPLETE */

/**

* The connection is done,

*/

What could be causing this? I wouldn't even know what code is actually relevant - the sheer amount of WPAN files is overwhelming and difficult to follow for a STM32WB newbie like myself.

Many thanks,

Jakub

This topic has been closed for replies.

1 reply

JakBSIP
JakBSIPAuthor
Associate II
Sep 9, 2021 9:22 AM UTC

I have noticed that aci_gap_create_connection() can take a garbage MAC address and still return BLE_STATUS_SUCCESS, so I suppose that flag simply indicates that all went well on the STM32 side and it is now trying to connect to some peripheral.

I have played a bit with the connection parameters as well, read the Bluetooth SIG for CSCP but to no avail.