Skip to main content
Associate
Jul 19, 2025 3:47 PM UTC
Solved

direct advertising stm32wb

i cant seem to really connect to my iphone after direct advertising i get a false print that i have connected

Bonded device 0 / 1 - Public BLE address xx:xx:xx:xx:xx:xx -- here it prints my true iphone bluetooth mac addr
aci_gap_add_devices_to_list() status = 0x00
aci_gap_get_bonded_devices = 0x00 (found 1 devices)
aci_gap_set_direct_connectable (HIGH DUTY) = 0x00
aci_gap_update_adv_data = 0x00
Directed ADV to iPhone = Success
>>== HCI_LE_ENHANCED_CONNECTION_COMPLETE_SUBEVT_CODE - Connection handle: 0x0
- Connection established with Central: @:4f:17:21:ee:cb:2c
- Connection Interval: 0.00 ms
- Connection latency: 0
- Supervision Timeout: 0 ms


it isnt truly connecting because i get the same print when my iphone is off or is not in range why does this happen?

i am using stm32wb15 nucleo board

i would love to get an example like this
https://github.com/stm32-hotspot/STM32WB-Filter-Accept-List-Peripheral

where the only change is that in 

static void adv_start(void)
it uses directed advertising instead of undirected

please help 
This topic has been closed for replies.
FilipKremen
FilipKremenBest answer
ST Employee
Jul 21, 2025 8:57 AM UTC

Hello,

according to Apple design guidelines, direct advertising towards iOS-based devices is not allowed.

Please visit this documentation below for more information.

Accessory Design Guidelines for Apple Devices

 

Best regards,

Filip Kremen

1 reply

FilipKremen
FilipKremenBest answer
ST Employee
Jul 21, 2025 8:57 AM UTC

Hello,

according to Apple design guidelines, direct advertising towards iOS-based devices is not allowed.

Please visit this documentation below for more information.

Accessory Design Guidelines for Apple Devices

 

Best regards,

Filip Kremen