Skip to main content
Associate III
Jun 25, 2024 11:20 AM UTC
Solved

Difference between app_subghz_phy.c and subghz_phy_app.c

Hello, I am working with RAK3172 which has STM32WLE5CCU6, from CubeMX I am enabling it's SUBGHZ_Phy functionality. But after code generation I am seeing there are two files "app_subghz_phy" and "subghz_phy_app", what are the differences between these two? Which files needs to be modified if I want to control the radio layer? Thank you.

This topic has been closed for replies.
STTwo-32
STTwo-32Best answer
ST Technical Moderator
Jun 26, 2024 1:29 PM UTC

OnTxDone, OnRxDone, OnTxTimeout,... are the functions to be executed depending on the values of the State variable. 

The Timers on the stm32_timer.c are based on the RTC.

Best Regards.

STTwo-32

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

4 replies

STTwo-32
ST Technical Moderator
Jun 25, 2024 12:23 PM UTC

Hello @pho3nix 

To control the radio layer on your application, you have to modify the "subghz_phy_app.c" and "subghz_phy_app.h". The "app_subghz_phy.c" is automatically generated when creating a Sub-GHz project.  It includes some initializations and configurations of the utilities that the wireless part may need. it includes also the function that run the sequencer of the project functions.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
pho3nixAuthor
Associate III
Jun 26, 2024 5:23 AM UTC

Ok, got it. One follow up question I had in mind, there are some functions like OnTxDone, OnRxDone, OnTxTimeout, OnRxTimeout, these are the callback functions in the app layer right?

 

Also, in the utility folder of the project, there is stm32_timer, what is the clock source for this timer, I couldn't find any proper resource so I am asking here.

STTwo-32
STTwo-32Best answer
ST Technical Moderator
Jun 26, 2024 1:29 PM UTC

OnTxDone, OnRxDone, OnTxTimeout,... are the functions to be executed depending on the values of the State variable. 

The Timers on the stm32_timer.c are based on the RTC.

Best Regards.

STTwo-32

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.