Skip to main content
GErma.1
Associate III
Apr 1, 2020 7:57 PM UTC
Question

Didisable TCXO on B-L072Z-LRWAN1 Discovery kit

Hi

There is any advantage in disabling the internal TCXO of the Lora Module by controlling the Pa12 pin?

BR

Gilberto

This topic has been closed for replies.

3 replies

Tesla DeLorean
Guru
Apr 1, 2020 10:05 PM UTC

Uses less power, turns the radio off (in as much as the SX1276 no longer gets clocked)

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
GErma.1
GErma.1Author
Associate III
Apr 2, 2020 6:42 PM UTC

Thanks

I have another question on a similar subject:

It is possible to provide a more accurate time base by connecting TCXO_OUT to PHO_OSC_IN according to the manual.

Can we switch the STM32L0 clock source dynamically between the internal oscillator and PHO_OSC_IN? If so I can use the internal oscillator during sleep mode and then switch to the external input for greater precision.

BR

Gilberto

Tesla DeLorean
Guru
Apr 2, 2020 6:56 PM UTC

Precision in doing what?

The radio uses the TCXO to get tight on band, and reduce the error budget. The MCU doesn't need to be clocked by the TCXO as generally the USART or I2C, for example are not that sensitive to slight clock error, whereas CAN or USB would be.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..