Skip to main content
Associate
Dec 19, 2025 5:21 AM UTC
Question

Debugging UART and BLE Advertising Issues on STM32WB05KZ (stm32cubewb0-v1-3-0)

I am currently working on BLE applications for a custom STM32WB05KZ board using the SDK stm32cubewb0-v1-3-0. In general, peripherals such as GPIO and UART are functioning correctly when running non-BLE examples provided in the SDK.

However, when I run BLE applications (such as Beacon, Server, or Client), I am unable to receive any logs over UART (configured on PB0 and PA1). I have verified that an LED, which is initialized prior to the BLE initialization in app_entry.c, operates correctly, indicating that the application is executing at least up to that point.

The main issues I am facing are:

  • No log output is observed on the UART interface during BLE operation.

  • The device does not appear to advertise(No address is visible: random or public), as it is not detected by the ST BLE Toolbox application.

I would appreciate any guidance or suggestions to help identify and resolve this issue.

1 reply

ST Technical Moderator
Dec 30, 2025 10:07 PM UTC
In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks