Skip to main content
Associate II
Mar 5, 2024 8:32 AM UTC
Question

Custom Clusters - transmit only valid attributes


Hello,

Currently, I am working with custom clusters, and I have a requirement related to transmitting and receiving the maximum number of attributes.

To illustrate, consider a cluster with three attributes:

Data Set - SET_0 
-------------------
Valid_data_set (True/False),
Attribute_A (<Attr_A_Data>) and
Attribute_B (<Attr_B_Data>)


which I interpret as SET_0 


Now, let's introduce three more data sets, SET_1 and SET_2.
In this setup, I have Zigbee Endpoints acting as servers, and the coordinator acts as the client, requesting these sets.


Question: I need to dynamically send data over these data sets. Specifically, I want to send data only if the Valid_data_set attribute of SET_0 is true. Similarly, I need to check and send in a single packet.
For example, if I have four sets with Valid_data_set attribute set to True out of a total of six sets, I want to send only those four sets of data to the coordinator upon a Zigbee request.
Suggestions and any other references are greatly appreciated.

--
Thanks,
Naani Ch 

This topic has been closed for replies.

1 reply

ST Employee
Mar 6, 2024 8:36 PM UTC

Hi All,

 

This question has been routed to our Online Support Center for direct support.

 

Regards,
Jake

ST Support