Custom board Stm32WBA65RIV6 no DFU connection
- 0 replies
- 206 views
Hello everyone,
I'm writing in search of some help, as I'm not sure what else to check.
I have just built a custom board controlled by an STM32WBA65RIV6, and I'm trying to connect it via DFU mode. Everything seems to be set up correctly, but the device is not detected by my computer (a MacBook).
What is working:
I can successfully flash the processor via ST-Link (SWD).
I have run a simple test program (toggling a pin high/low every 3 seconds) without issues. This confirms the chip is alive and basic operation is fine.
DFU Setup & Debugging Steps Taken:
The BOOT0 pin is pulled up to 3.3V with a 10k resistor to enter the system bootloader (DFU).
I've confirmed this works: when BOOT0 is high, my test program does not run. When BOOT0 is pulled low, the program runs. This confirms the boot mode selection is working as intended.
I have double-checked the D- (Data Minus) and D+ (Data Plus) lines for continuity and to ensure they are not swapped.
I also (after initially forgetting) manually connected the USB_OTG_VBUS pin to the 3.3V line from the USB connector.
I am using a known-good USB data cable (not just a charging cable).
Despite these steps, my MacBook still cannot find the board. I have attached photos of my USB circuit schematic for review.
My Questions:
Am I missing a required connection?
Do I need to configure any special settings (e.g., option bytes) via ST-Link before DFU will work?
Has anyone else experienced issues using DFU with this chip, particularly on a MacBook?
I'm a bit lost on what to check next and would appreciate any suggestions.
Thank you in advance! :handshake: