Skip to main content
PLaid.1
Associate II
May 14, 2025 8:34 PM UTC
Question

CubeWL LoRaWAN End_Node example wont connect to Chirpstack due to Nonce

I'm developing LoRaWan project using that uses STM32WL5MOC module and the STM32CubeWL MCU Package (STM32Cube_FW_WL_V1.3.0). I have B-WL5M-SUBG1 module to develop with.

I am seeing that the End Node example does not connect with Chirpstack due to noncompliant DevNonce.  It seems I need to patch ST’s CubeWL LoRaWAN End_Node example to make DevNonce persistent across power cycles so that ChirpStack will accept joins).

Has anyone else experienced this?  Any insights are welcomed.

Peter

 

This topic has been closed for replies.

1 reply

STTwo-32
ST Technical Moderator
May 14, 2025 8:47 PM UTC

Hello @PLaid.1 

I suggest you to have a look at this article from Digikey. It gives a description on how to connect the STM32WL to the ChirpStack.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.